<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC5528 USB_DEVICE_CONFIG_ENDPOINTS value</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB-DEVICE-CONFIG-ENDPOINTS-value/m-p/1795754#M55238</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a small question about the USB_DEVICE_CONFIG_ENDPOINTS value setting. From the comment in the code, I can see that it might be the value of how many endpoints are supported in the stack.&lt;/P&gt;&lt;P&gt;However, from the content in USB_DeviceInitEndpoint and USB_DeviceInit, I think the value should be the &lt;FONT color="#FF0000"&gt;maximum logical endpoint index&lt;/FONT&gt; we need in the project.&lt;/P&gt;&lt;P&gt;Which one is correct?&lt;/P&gt;&lt;P&gt;And if I only have two endpoints, which are endpoint 3 in and out, should I set USB_DEVICE_CONFIG_ENDPOINTS to 4 (maximum logical endpoint index + 1)?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Peter&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jan 2024 03:31:24 GMT</pubDate>
    <dc:creator>tks11111</dc:creator>
    <dc:date>2024-01-26T03:31:24Z</dc:date>
    <item>
      <title>LPC5528 USB_DEVICE_CONFIG_ENDPOINTS value</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB-DEVICE-CONFIG-ENDPOINTS-value/m-p/1795754#M55238</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a small question about the USB_DEVICE_CONFIG_ENDPOINTS value setting. From the comment in the code, I can see that it might be the value of how many endpoints are supported in the stack.&lt;/P&gt;&lt;P&gt;However, from the content in USB_DeviceInitEndpoint and USB_DeviceInit, I think the value should be the &lt;FONT color="#FF0000"&gt;maximum logical endpoint index&lt;/FONT&gt; we need in the project.&lt;/P&gt;&lt;P&gt;Which one is correct?&lt;/P&gt;&lt;P&gt;And if I only have two endpoints, which are endpoint 3 in and out, should I set USB_DEVICE_CONFIG_ENDPOINTS to 4 (maximum logical endpoint index + 1)?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Peter&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jan 2024 03:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB-DEVICE-CONFIG-ENDPOINTS-value/m-p/1795754#M55238</guid>
      <dc:creator>tks11111</dc:creator>
      <dc:date>2024-01-26T03:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB_DEVICE_CONFIG_ENDPOINTS value</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB-DEVICE-CONFIG-ENDPOINTS-value/m-p/1813169#M55485</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Full-Speed (FS) USB device supports 10 physical endpoints and High-Speed (HS) USB device supports 12 physical endpoints. You could refer to &lt;EM&gt;Table 763. Fixed endpoint configuration&lt;/EM&gt; and &lt;EM&gt;Table 831. Fixed endpoint configuration&lt;/EM&gt; from user manual for more detail.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 22:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB-DEVICE-CONFIG-ENDPOINTS-value/m-p/1813169#M55485</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-02-21T22:04:09Z</dc:date>
    </item>
  </channel>
</rss>