<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Is the Universal Multilink (PEmicro) programmer is compatible with the LPC5504JHI48QL?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-Universal-Multilink-PEmicro-programmer-is-compatible-with/m-p/1789558#M55160</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Eletronicc_23&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Please make sure UMultilink firmware is the latest and supporting LPC&lt;/P&gt;
&lt;P&gt;2. When UMultilink connects baord, are both of the leds on multilink on?&lt;/P&gt;
&lt;P&gt;3. LPC55 debug uses SWD interface, please refer below article for SWD interface design.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jan 2024 14:12:31 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2024-01-16T14:12:31Z</dc:date>
    <item>
      <title>Is the Universal Multilink (PEmicro) programmer is compatible with the LPC5504JHI48QL?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-Universal-Multilink-PEmicro-programmer-is-compatible-with/m-p/1789321#M55151</link>
      <description>&lt;P&gt;Hi my friends, I have this doubt because I did the connection of the programmer with the pins of the microcontroller that we need use to load the program using the MCUXpresso IDE&lt;/P&gt;&lt;P&gt;The pins of the program that I used of the programmer PEmicro with the microcontroller&amp;nbsp; LPC5504JHI48QL are the follows:&lt;/P&gt;&lt;P&gt;* Pin 2 TMS/SWD_DIO&amp;nbsp;of the programmer PEmicro with the Pin 43 PIO_4/TMS of the microcontroller.&lt;/P&gt;&lt;P&gt;* Pin 4 TCK/SWD_CLK of the programmer PEmicro with the Pin 41 PIO_3/TCK of the microcontroller.&lt;/P&gt;&lt;P&gt;* Pin 6 TDO of the programmer PEmicro with the Pin 45 Pin PIO_6/TDO of the microcontroller.&lt;/P&gt;&lt;P&gt;* Pin 8 TDI of the programmer PEmicro with the Pin 44 PIO_5/ TDI of the microcontroller.&lt;/P&gt;&lt;P&gt;* Pin 10 of the RESET of the programmer PEmicro with the PIN 19 RESETN of the microcontroller&lt;/P&gt;&lt;P&gt;Those are all the connections that I did of the programmer with the microcontroller, and when I try to debug with thE MCUXpresso Ide, it is not working nothing. Also I checked the 3.3v voltage in the microcontroller that is the voltage it is need to work and it is ok.&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;* Are the connections that I did of the programmer with the microcontroller are ok?&lt;/P&gt;&lt;P&gt;* Does this connection need something else to make it works without any problem and start to debug with the IDE?&lt;/P&gt;&lt;P&gt;Thank you so much friends,&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 08:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-Universal-Multilink-PEmicro-programmer-is-compatible-with/m-p/1789321#M55151</guid>
      <dc:creator>Eletronicc_23</dc:creator>
      <dc:date>2024-01-16T08:45:31Z</dc:date>
    </item>
    <item>
      <title>Re: Is the Universal Multilink (PEmicro) programmer is compatible with the LPC5504JHI48QL?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-Universal-Multilink-PEmicro-programmer-is-compatible-with/m-p/1789558#M55160</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Eletronicc_23&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Please make sure UMultilink firmware is the latest and supporting LPC&lt;/P&gt;
&lt;P&gt;2. When UMultilink connects baord, are both of the leds on multilink on?&lt;/P&gt;
&lt;P&gt;3. LPC55 debug uses SWD interface, please refer below article for SWD interface design.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 14:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-Universal-Multilink-PEmicro-programmer-is-compatible-with/m-p/1789558#M55160</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2024-01-16T14:12:31Z</dc:date>
    </item>
  </channel>
</rss>