<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC54S016JBD100 Valid Address Mac in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S016JBD100-Valid-Address-Mac/m-p/1787420#M55131</link>
    <description>&lt;P&gt;My application will be responsible for propagating the telemetry of my equipment to some systems. For this I will use an LPC54S016JBD100 that already has an Ethernet PHY. In order for me to place my equipment on my clients' network, via DNS or fixed IP, I will need a valid MAC ADDRESS according to EUI-48, I would like to know if the LPC54S016JBD100 already comes with a MAC ADDRESS from the factory and if it does, is it unique? for each microcontroller?&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jan 2024 18:11:57 GMT</pubDate>
    <dc:creator>worosco</dc:creator>
    <dc:date>2024-01-11T18:11:57Z</dc:date>
    <item>
      <title>LPC54S016JBD100 Valid Address Mac</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S016JBD100-Valid-Address-Mac/m-p/1787420#M55131</link>
      <description>&lt;P&gt;My application will be responsible for propagating the telemetry of my equipment to some systems. For this I will use an LPC54S016JBD100 that already has an Ethernet PHY. In order for me to place my equipment on my clients' network, via DNS or fixed IP, I will need a valid MAC ADDRESS according to EUI-48, I would like to know if the LPC54S016JBD100 already comes with a MAC ADDRESS from the factory and if it does, is it unique? for each microcontroller?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 18:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S016JBD100-Valid-Address-Mac/m-p/1787420#M55131</guid>
      <dc:creator>worosco</dc:creator>
      <dc:date>2024-01-11T18:11:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54S016JBD100 Valid Address Mac</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S016JBD100-Valid-Address-Mac/m-p/1787617#M55132</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As the section 37.6.28 MAC address high register in UM11060.pdf, there are two mac registers to save 48 bits mac address: MAC_ADDR_HIGH and MAC_ADDR_LOW, the MAC_ADDR_LOW saves 32 bits low mac address, the MAC_ADDR_HIGH saves high 16 bits mac address.&lt;/P&gt;
&lt;P&gt;It is required for user to assign mac address to the mac address register with firmware, there is not default value for the two registers.&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1705025856758.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257861i1E27FCA027A7C093/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1705025856758.png" alt="xiangjun_rong_0-1705025856758.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1705025856758.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 02:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S016JBD100-Valid-Address-Mac/m-p/1787617#M55132</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-01-12T02:22:27Z</dc:date>
    </item>
  </channel>
</rss>