<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problems with high speed USB enumeration on LPC1823 custom hardware in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/1786971#M55128</link>
    <description>&lt;P&gt;When running our firmware on the LPC18S37 DVK the board enumerates over USB as high speed successfully.&lt;/P&gt;&lt;P&gt;Running the same firmware on our custom hardware the board enumerates as full speed.&lt;/P&gt;&lt;P&gt;We're using USB0.&lt;BR /&gt;On the scope, we don't see the chirp sequence prior to enumeration as if the board isn't attempting to enumerate as high speed.&lt;/P&gt;&lt;P&gt;We've removed all components on USB data lines between connector and MCU and see the same problem.&lt;/P&gt;&lt;P&gt;Have looked at the USB errata for LPC18xx and can't see anything that would cause this.&lt;/P&gt;&lt;P&gt;Have stepped through code prior to enumeration and setup in the USB registers looks correct to me.&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jan 2024 07:53:42 GMT</pubDate>
    <dc:creator>MarkDale</dc:creator>
    <dc:date>2024-01-11T07:53:42Z</dc:date>
    <item>
      <title>Problems with high speed USB enumeration on LPC1823 custom hardware</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/1786971#M55128</link>
      <description>&lt;P&gt;When running our firmware on the LPC18S37 DVK the board enumerates over USB as high speed successfully.&lt;/P&gt;&lt;P&gt;Running the same firmware on our custom hardware the board enumerates as full speed.&lt;/P&gt;&lt;P&gt;We're using USB0.&lt;BR /&gt;On the scope, we don't see the chirp sequence prior to enumeration as if the board isn't attempting to enumerate as high speed.&lt;/P&gt;&lt;P&gt;We've removed all components on USB data lines between connector and MCU and see the same problem.&lt;/P&gt;&lt;P&gt;Have looked at the USB errata for LPC18xx and can't see anything that would cause this.&lt;/P&gt;&lt;P&gt;Have stepped through code prior to enumeration and setup in the USB registers looks correct to me.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 07:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/1786971#M55128</guid>
      <dc:creator>MarkDale</dc:creator>
      <dc:date>2024-01-11T07:53:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with high speed USB enumeration on LPC1823 custom hardware</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/1790062#M55165</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If the firmware is the same, have you compared the schematics design?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 07:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/1790062#M55165</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-01-17T07:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with high speed USB enumeration on LPC1823 custom hardware</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/2055570#M57816</link>
      <description>&lt;P&gt;Thanks for your response. Sorry for the slow reply.&lt;BR /&gt;In the end, we had missed out the USB0_RREF resistor in our schematic design (see attached table from reference manual).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="usbref.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/326696iEB1C709F987C7625/image-size/medium?v=v2&amp;amp;px=400" role="button" title="usbref.png" alt="usbref.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;High speed USB comms now working as expected. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 14:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problems-with-high-speed-USB-enumeration-on-LPC1823-custom/m-p/2055570#M57816</guid>
      <dc:creator>MarkDale</dc:creator>
      <dc:date>2025-03-04T14:25:33Z</dc:date>
    </item>
  </channel>
</rss>