<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does LPC54628 support more than one ethernet PHY? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-LPC54628-support-more-than-one-ethernet-PHY/m-p/1785489#M55117</link>
    <description>&lt;P&gt;The pinout of the MCU suggests that there are enough pins to set up two ethernet PHYs. Is this possible? For example read sensor data from two ethernet based sensors without setting up an intermediate switch.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Jan 2024 19:53:04 GMT</pubDate>
    <dc:creator>PLM</dc:creator>
    <dc:date>2024-01-09T19:53:04Z</dc:date>
    <item>
      <title>Does LPC54628 support more than one ethernet PHY?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-LPC54628-support-more-than-one-ethernet-PHY/m-p/1785489#M55117</link>
      <description>&lt;P&gt;The pinout of the MCU suggests that there are enough pins to set up two ethernet PHYs. Is this possible? For example read sensor data from two ethernet based sensors without setting up an intermediate switch.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 19:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-LPC54628-support-more-than-one-ethernet-PHY/m-p/1785489#M55117</guid>
      <dc:creator>PLM</dc:creator>
      <dc:date>2024-01-09T19:53:04Z</dc:date>
    </item>
    <item>
      <title>Re: Does LPC54628 support more than one ethernet PHY?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-LPC54628-support-more-than-one-ethernet-PHY/m-p/1785986#M55125</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227945"&gt;@PLM&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try to connect two, but, only can can used at the same time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 10:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-LPC54628-support-more-than-one-ethernet-PHY/m-p/1785986#M55125</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-01-10T10:01:44Z</dc:date>
    </item>
  </channel>
</rss>