<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Sleep mode dma wake up</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sleep-mode-dma-wake-up/m-p/1781342#M55085</link>
    <description>&lt;P&gt;Hi community ,&lt;BR /&gt;I'm working on the Sleep modes of the NXP LPC55S69 board.&lt;BR /&gt;I'm trying to wake up the system using uart2 which is configurated as DMA will the DMA IRQ wake up the device or I need to Configure the Flexcomm as the Interrupt or the DMA irq will work ??&lt;BR /&gt;Device used LPC55S69&lt;BR /&gt;Sleep mode wake up using flexcomm2&lt;BR /&gt;Thank you and regards&amp;nbsp;&lt;BR /&gt;UJWAL&lt;/P&gt;</description>
    <pubDate>Mon, 01 Jan 2024 13:22:03 GMT</pubDate>
    <dc:creator>ujwal_kumar_N_L</dc:creator>
    <dc:date>2024-01-01T13:22:03Z</dc:date>
    <item>
      <title>Sleep mode dma wake up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sleep-mode-dma-wake-up/m-p/1781342#M55085</link>
      <description>&lt;P&gt;Hi community ,&lt;BR /&gt;I'm working on the Sleep modes of the NXP LPC55S69 board.&lt;BR /&gt;I'm trying to wake up the system using uart2 which is configurated as DMA will the DMA IRQ wake up the device or I need to Configure the Flexcomm as the Interrupt or the DMA irq will work ??&lt;BR /&gt;Device used LPC55S69&lt;BR /&gt;Sleep mode wake up using flexcomm2&lt;BR /&gt;Thank you and regards&amp;nbsp;&lt;BR /&gt;UJWAL&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jan 2024 13:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sleep-mode-dma-wake-up/m-p/1781342#M55085</guid>
      <dc:creator>ujwal_kumar_N_L</dc:creator>
      <dc:date>2024-01-01T13:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: Sleep mode dma wake up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sleep-mode-dma-wake-up/m-p/1781552#M55089</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221323"&gt;@ujwal_kumar_N_L&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, need enable DMA interrupt before enter sleep mode, then&amp;nbsp; DMA interrupt will wake up cpu.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 08:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sleep-mode-dma-wake-up/m-p/1781552#M55089</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-01-02T08:23:22Z</dc:date>
    </item>
  </channel>
</rss>