<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VCOM driver for LPC1549 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1780170#M55060</link>
    <description>&lt;P&gt;I downloaded the LPCOpen to use the smple code of VCOM function for LPC1549.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.jp/design/design-center/software/software-library/lpcopen-software-development-platform-lpc15xx:LPCOPEN-SOFTWARE-FOR-LPC15XX" target="_blank"&gt;LPCOpen Software for LPC15XX | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;&lt;P&gt;In the readme.txt, inf file is needed when I connect to the Windows host.&lt;/P&gt;&lt;P&gt;But I couldn't find the .inf file in LPCOpen zip file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;*Special connection requirements:&lt;BR /&gt;--------------------------------&lt;BR /&gt;Connect the USB cable between micro connector on board and to a host.&lt;BR /&gt;When connected to Windows host use the .inf included in the project&lt;BR /&gt;directory to install the driver. For OSx (Mac) host, no drivers are needed.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Where is the .inf file ?&amp;nbsp; or Where is the download link in the HP?&lt;/P&gt;&lt;P&gt;I'd like the help and information..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Dec 2023 00:47:48 GMT</pubDate>
    <dc:creator>emitterLCR</dc:creator>
    <dc:date>2023-12-27T00:47:48Z</dc:date>
    <item>
      <title>VCOM driver for LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1780170#M55060</link>
      <description>&lt;P&gt;I downloaded the LPCOpen to use the smple code of VCOM function for LPC1549.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.jp/design/design-center/software/software-library/lpcopen-software-development-platform-lpc15xx:LPCOPEN-SOFTWARE-FOR-LPC15XX" target="_blank"&gt;LPCOpen Software for LPC15XX | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;&lt;P&gt;In the readme.txt, inf file is needed when I connect to the Windows host.&lt;/P&gt;&lt;P&gt;But I couldn't find the .inf file in LPCOpen zip file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;*Special connection requirements:&lt;BR /&gt;--------------------------------&lt;BR /&gt;Connect the USB cable between micro connector on board and to a host.&lt;BR /&gt;When connected to Windows host use the .inf included in the project&lt;BR /&gt;directory to install the driver. For OSx (Mac) host, no drivers are needed.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Where is the .inf file ?&amp;nbsp; or Where is the download link in the HP?&lt;/P&gt;&lt;P&gt;I'd like the help and information..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 00:47:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1780170#M55060</guid>
      <dc:creator>emitterLCR</dc:creator>
      <dc:date>2023-12-27T00:47:48Z</dc:date>
    </item>
    <item>
      <title>Re: VCOM driver for LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1780261#M55063</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;i suppose that the *.inf file for USB is defined/saved/run in PC side instead of MCU side, generally, you can use default *.inf file.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 05:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1780261#M55063</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-12-27T05:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: VCOM driver for LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1783254#M55098</link>
      <description>&lt;P&gt;Sorry for replying late.&lt;/P&gt;&lt;P&gt;I could use the standard driver on Windows.&lt;/P&gt;&lt;P&gt;The driver was installed automatically.&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 00:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/VCOM-driver-for-LPC1549/m-p/1783254#M55098</guid>
      <dc:creator>emitterLCR</dc:creator>
      <dc:date>2024-01-05T00:32:33Z</dc:date>
    </item>
  </channel>
</rss>