<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックJump to USB_Connect boot from code</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779387#M55045</link>
    <description>&lt;P&gt;OK This is probably impossible, but is there a way when running code, to jump to the rom bootloader and get it into USB Connect, to easily do an upgrade from the USB port?&lt;/P&gt;</description>
    <pubDate>Sat, 23 Dec 2023 02:30:47 GMT</pubDate>
    <dc:creator>jimc</dc:creator>
    <dc:date>2023-12-23T02:30:47Z</dc:date>
    <item>
      <title>Jump to USB_Connect boot from code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779387#M55045</link>
      <description>&lt;P&gt;OK This is probably impossible, but is there a way when running code, to jump to the rom bootloader and get it into USB Connect, to easily do an upgrade from the USB port?&lt;/P&gt;</description>
      <pubDate>Sat, 23 Dec 2023 02:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779387#M55045</guid>
      <dc:creator>jimc</dc:creator>
      <dc:date>2023-12-23T02:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: Jump to USB_Connect boot from code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779671#M55048</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/118817"&gt;@jimc&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It can jump to UART_ISP mode through "Reinvoke ISP":&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1703495709902.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255799i8282CCA9B435D879/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1703495709902.png" alt="Alice_Yang_0-1703495709902.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1703495709902.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Dec 2023 09:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779671#M55048</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-12-25T09:15:18Z</dc:date>
    </item>
    <item>
      <title>Re: Jump to USB_Connect boot from code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779758#M55052</link>
      <description>THANKS!!!!!</description>
      <pubDate>Mon, 25 Dec 2023 14:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Jump-to-USB-Connect-boot-from-code/m-p/1779758#M55052</guid>
      <dc:creator>jimc</dc:creator>
      <dc:date>2023-12-25T14:47:36Z</dc:date>
    </item>
  </channel>
</rss>