<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NFC in phones in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-in-phones/m-p/1778402#M55025</link>
    <description>&lt;P&gt;Hi community&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on NFC&amp;nbsp; RC663 ,i have tried reading NFC tags and cards .Im unable to use phone as a card emulator. The NFC id&amp;nbsp; keeps on changing as the NFC in phones is used for contactless paying .Is there anyway in which i can use some mobile application and make sure the phone send the same id all the time?&lt;BR /&gt;Application is that phone acts as a method of accessing the door system .So i need the ID to be constant .&lt;/P&gt;&lt;P&gt;Thank you and regards&amp;nbsp;&lt;BR /&gt;UJWAL&lt;/P&gt;</description>
    <pubDate>Thu, 21 Dec 2023 06:13:57 GMT</pubDate>
    <dc:creator>ujwal_kumar_N_L</dc:creator>
    <dc:date>2023-12-21T06:13:57Z</dc:date>
    <item>
      <title>NFC in phones</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-in-phones/m-p/1778402#M55025</link>
      <description>&lt;P&gt;Hi community&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on NFC&amp;nbsp; RC663 ,i have tried reading NFC tags and cards .Im unable to use phone as a card emulator. The NFC id&amp;nbsp; keeps on changing as the NFC in phones is used for contactless paying .Is there anyway in which i can use some mobile application and make sure the phone send the same id all the time?&lt;BR /&gt;Application is that phone acts as a method of accessing the door system .So i need the ID to be constant .&lt;/P&gt;&lt;P&gt;Thank you and regards&amp;nbsp;&lt;BR /&gt;UJWAL&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 06:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-in-phones/m-p/1778402#M55025</guid>
      <dc:creator>ujwal_kumar_N_L</dc:creator>
      <dc:date>2023-12-21T06:13:57Z</dc:date>
    </item>
    <item>
      <title>Re: NFC in phones</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-in-phones/m-p/1778919#M55036</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I apologize for the inconveniences.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 22:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-in-phones/m-p/1778919#M55036</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2023-12-21T22:47:25Z</dc:date>
    </item>
  </channel>
</rss>