<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: MCUXpresso J-Link encountered a problem for LPC865</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774621#M54953</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Because the LPC86x is a newly released sub-family, it is possible that the J-Link device from Segger does not support it.&lt;/P&gt;
&lt;P&gt;Pls ask Segger support&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 14 Dec 2023 08:51:02 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-12-14T08:51:02Z</dc:date>
    <item>
      <title>MCUXpresso J-Link encountered a problem for LPC865</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1773310#M54933</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I have a problem to run MCUXpresso with J-Link for my target board with LPC865.&lt;BR /&gt;Error message tells that "JLink Debug has encountered a problem".&lt;BR /&gt;As I looked into J-Link Debug Settings, it does not seem that JLink Debugger Settings of MCUXpresso has appropriate device.&lt;BR /&gt;I have set "Cortex-M0+" as device type in my JLink Debug SettingsFile.jlink because target device settings list of SEGGER J-Link V7.88 has it , but no LPC865 (or representative), however that does not work.&lt;/P&gt;&lt;P&gt;For your better understanding my case;&lt;BR /&gt;1. MCUXpresso version: v11.8.0&lt;BR /&gt;2. J-Link version: v7.88m (2023-07-19)&lt;BR /&gt;3. MCU: LPC865M201&lt;BR /&gt;4. attached you will see screen capture of;&lt;BR /&gt;a. JLink Debugger settings&lt;BR /&gt;b. target device settings list of SEGGER J-Link V7.88&lt;BR /&gt;c. JLink Debug SettingsFile.jlink&lt;BR /&gt;&lt;BR /&gt;Please let me know how to get the appropriate device of LPC865 for MCUXpresso with J-Link.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 18:08:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1773310#M54933</guid>
      <dc:creator>uzza9</dc:creator>
      <dc:date>2023-12-12T18:08:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso J-Link encountered a problem for LPC865</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1773495#M54937</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you use LPCXpresso860-Max board and MCUXPresso tools.&lt;/P&gt;
&lt;P&gt;In the case, you can connect the J4 usb connector to PC,then delete the *Debug.launch file, which can be generated automatically.&lt;/P&gt;
&lt;P&gt;Then click "Debug", the MCUXPresso tools can detect the correct probe you connected, and download.&lt;/P&gt;
&lt;P&gt;If you use your own board and true J-Link device from Segger, I am sorry.&lt;/P&gt;
&lt;P&gt;If you use LPCXpresso860-Max board and J-Link device from Segger, you have to close JP1, connect the J-Link device to J7.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1702433603744.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254069i028D3EA652A612D0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1702433603744.png" alt="xiangjun_rong_0-1702433603744.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1702433603744.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 02:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1773495#M54937</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-12-13T02:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso J-Link encountered a problem for LPC865</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774117#M54944</link>
      <description>&lt;P&gt;Hello XiangJun Rong,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your clarification.&lt;/P&gt;&lt;P&gt;It sounds like I CAN NOT use the Segger J-link probe (I am trying to use J-Link Base) for my custom board with LPC865. My team&amp;nbsp;developed the custom board by referring to &lt;SPAN&gt;LPCXpresso860-Max board&lt;/SPAN&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For your information, I have been using P&amp;amp;E Multilink Universal probe for my custom board debugging without problem. However I am trying to use Segger J-Link probe so that I can do "attach to running target" option that does not seem to work with P&amp;amp;E Multilink probe.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My new question, is there a way to "attach to running target" (or similar) for the P&amp;amp;E probe?&lt;/P&gt;&lt;P&gt;By the way, I attached pop up error message of "Unable to find device LPC865" that I ran into while connecting the Segger probe to my custom board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It will be appreciated if you provide me any technical tip to resolve this issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 17:27:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774117#M54944</guid>
      <dc:creator>uzza9</dc:creator>
      <dc:date>2023-12-13T17:27:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso J-Link encountered a problem for LPC865</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774621#M54953</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Because the LPC86x is a newly released sub-family, it is possible that the J-Link device from Segger does not support it.&lt;/P&gt;
&lt;P&gt;Pls ask Segger support&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 08:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774621#M54953</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-12-14T08:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso J-Link encountered a problem for LPC865</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774896#M54963</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;XiangJun Rong,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I got clear and thank you for your clarification that saves my effort to struggle the J-Link to my target with LPC865.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 15:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-J-Link-encountered-a-problem-for-LPC865/m-p/1774896#M54963</guid>
      <dc:creator>uzza9</dc:creator>
      <dc:date>2023-12-14T15:04:54Z</dc:date>
    </item>
  </channel>
</rss>