<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Issue with LCD display Interface on LPC54618J512BD208</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774604#M54952</link>
    <description>&lt;P&gt;&lt;EM&gt;&amp;gt; When I attempt to display text, it does not appear as expected. Interestingly, the color blue displays correctly, but other colors do not seem to work.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think the problem is in your code.&lt;BR /&gt;Check the color mode you are using, and alignment of the respective bitfields in one color RAM word.&lt;BR /&gt;Like, one of the common 16-bit color modes used in LCDs is 5-6-5 (RGB).&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 14 Dec 2023 08:43:29 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2023-12-14T08:43:29Z</dc:date>
    <item>
      <title>Issue with LCD display Interface on LPC54618J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774520#M54950</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am currently engaged in a project that involves the use of the LPC54618J512BD208 microcontroller. I am facing a challenge with the interface of the LCD display(G057VN01V2).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I attempt to display text, it does not appear as expected. Interestingly, the color blue displays correctly, but other colors do not seem to work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The SDRAM part number for reference is IS42S32160D-5BL.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For further clarity, I am attaching the configurations of both the LCD and SDRAM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any help or suggestions would be greatly appreciated.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 07:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774520#M54950</guid>
      <dc:creator>nithin3200</dc:creator>
      <dc:date>2023-12-14T07:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LCD display Interface on LPC54618J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774604#M54952</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; When I attempt to display text, it does not appear as expected. Interestingly, the color blue displays correctly, but other colors do not seem to work.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think the problem is in your code.&lt;BR /&gt;Check the color mode you are using, and alignment of the respective bitfields in one color RAM word.&lt;BR /&gt;Like, one of the common 16-bit color modes used in LCDs is 5-6-5 (RGB).&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 08:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774604#M54952</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-12-14T08:43:29Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LCD display Interface on LPC54618J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774731#M54956</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your response. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am proceeding in the same manner as you suggested. If you could review my LCD and SDRAM configurations, you might understand the situation better. For further clarity, I am also attaching the clock configuration&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 10:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1774731#M54956</guid>
      <dc:creator>nithin3200</dc:creator>
      <dc:date>2023-12-14T10:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LCD display Interface on LPC54618J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1775327#M54966</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203985"&gt;@nithin3200&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-align-justify" style="text-align: justify; text-justify: inter-ideograph; text-indent: 21.0pt; background: white; margin: 0cm 0cm 11.25pt 0cm;"&gt;&lt;SPAN&gt;Hello, we recommend that you use GUI Guider software for design, after the generation of the code for a simple port, you can display the effect you want.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P class="lia-align-justify" style="text-align: justify; text-justify: inter-ideograph; background: white; margin: 0cm 0cm 11.25pt 0cm;"&gt;&lt;SPAN&gt;Best regards, Alex.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 06:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1775327#M54966</guid>
      <dc:creator>Alex_Wang</dc:creator>
      <dc:date>2023-12-15T06:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LCD display Interface on LPC54618J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1775374#M54967</link>
      <description>&lt;P&gt;I wouldn't think it is a clock issue if at least one color is displayed correctly.&lt;/P&gt;&lt;P&gt;As a side note, I am not an NXP employee or have any such board currently, so I have neither the time nor the hardware to get too deep into your issues. But I can share my experiences.&lt;/P&gt;&lt;P&gt;Having dealt with LCD display controllers in the past, the sparingly documented register interface can be a challenge and usually requires some experimentation. The applies to both geometry (sizes &amp;amp; orientation) and colors.&lt;BR /&gt;For the geometry settings, I used to draw a diagonal line onto the display (just increment x and y coordinated simultaneously.&lt;BR /&gt;For color, I used lines/blocks of one primary color (R, G or B), side by side. Intensity variations and gradients follow afterwards.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 07:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1775374#M54967</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-12-15T07:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LCD display Interface on LPC54618J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1778620#M55034</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203985"&gt;@nithin3200&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is a demo and AN can refer to:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12027.zip?_gl=1*1ovo166*_ga*MTI4OTk1OTg5MC4xNzAzMTUwNjY1*_ga_WM5LE0KMSH*MTcwMzE1MDY2NS4xLjAuMTcwMzE1MDY2OS4wLjAuMA.." target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/nxp/application-notes/AN12027.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 09:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Issue-with-LCD-display-Interface-on-LPC54618J512BD208/m-p/1778620#M55034</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-12-21T09:26:04Z</dc:date>
    </item>
  </channel>
</rss>