<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC5410x Errata : POWER_API.1 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Errata-POWER-API-1/m-p/1768846#M54874</link>
    <description>&lt;P&gt;There is a section in the LPC5410x Errata Sheet (ES_LPC5410x) entitled: "POWER_API.1: The set-voltage API ROM call does not configure the internal regulator correctly for the desired operating frequency"&lt;/P&gt;&lt;P&gt;The stated workaround is the use the power_lib library in LPCOpen v3.xx when setting voltage for a given frequency.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on NXP guidance, we are using the MCUxpresso SDK instead of the LPCOpen SDK for our LPC54102 project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the&amp;nbsp;POWER_SetVoltageForFreq() function in the MCUXpresso SDK safe to use? In other words, is it implemented such that it avoids the issue described in the errata sheet?&lt;/P&gt;</description>
    <pubDate>Tue, 05 Dec 2023 08:08:24 GMT</pubDate>
    <dc:creator>BTaylor</dc:creator>
    <dc:date>2023-12-05T08:08:24Z</dc:date>
    <item>
      <title>LPC5410x Errata : POWER_API.1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Errata-POWER-API-1/m-p/1768846#M54874</link>
      <description>&lt;P&gt;There is a section in the LPC5410x Errata Sheet (ES_LPC5410x) entitled: "POWER_API.1: The set-voltage API ROM call does not configure the internal regulator correctly for the desired operating frequency"&lt;/P&gt;&lt;P&gt;The stated workaround is the use the power_lib library in LPCOpen v3.xx when setting voltage for a given frequency.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on NXP guidance, we are using the MCUxpresso SDK instead of the LPCOpen SDK for our LPC54102 project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the&amp;nbsp;POWER_SetVoltageForFreq() function in the MCUXpresso SDK safe to use? In other words, is it implemented such that it avoids the issue described in the errata sheet?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 08:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Errata-POWER-API-1/m-p/1768846#M54874</guid>
      <dc:creator>BTaylor</dc:creator>
      <dc:date>2023-12-05T08:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5410x Errata : POWER_API.1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Errata-POWER-API-1/m-p/1769413#M54888</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that it is safe to use the void POWER_SetVoltageForFreq(uint32_t freq); which is defined in the fsl_power.h, the api function can set up LDO output voltage based on core frequency.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 02:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Errata-POWER-API-1/m-p/1769413#M54888</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-12-06T02:53:11Z</dc:date>
    </item>
  </channel>
</rss>