<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC5528 USB1 as full speed device in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-as-full-speed-device/m-p/1767279#M54857</link>
    <description>&lt;P&gt;HI&amp;nbsp;tks11111,&lt;/P&gt;
&lt;P&gt;There is no need setting clock.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;To set LPC5528 USB1 as full speed device, setting&amp;nbsp;&lt;EM&gt;Forced FS&lt;/EM&gt; bit as 1 is enough.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Dec 2023 12:21:43 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2023-12-01T12:21:43Z</dc:date>
    <item>
      <title>LPC5528 USB1 as full speed device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-as-full-speed-device/m-p/1759618#M54750</link>
      <description>&lt;P&gt;Hi All,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found a thread that discussed how to use USB1 as a full-speed device.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-USB1-as-full-speed-device/td-p/1680697" target="_blank" rel="noopener"&gt;LPC55S6x USB1 as full speed device - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Do I need to change the clock setting if I set the bit 21 of the USB1 device command/status register (DEVCMDSTAT) to 1?&lt;BR /&gt;Also, do I need to add any other speed configuration?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Appreciate any help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Peter&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 06:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-as-full-speed-device/m-p/1759618#M54750</guid>
      <dc:creator>tks11111</dc:creator>
      <dc:date>2023-11-20T06:52:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1 as full speed device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-as-full-speed-device/m-p/1767279#M54857</link>
      <description>&lt;P&gt;HI&amp;nbsp;tks11111,&lt;/P&gt;
&lt;P&gt;There is no need setting clock.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;To set LPC5528 USB1 as full speed device, setting&amp;nbsp;&lt;EM&gt;Forced FS&lt;/EM&gt; bit as 1 is enough.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 12:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-as-full-speed-device/m-p/1767279#M54857</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-12-01T12:21:43Z</dc:date>
    </item>
  </channel>
</rss>