<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC5528 Force USB1 as Full speed Device</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1766399#M54841</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Alice,&lt;/P&gt;&lt;P&gt;Thanks for the quick reply.&lt;/P&gt;&lt;P&gt;I had a quick question. If I want to toggle the USB1 between High Speed and Full Speed, I need to&lt;/P&gt;&lt;P&gt;call NVIC_SystemReset() and then toggle the Forced FS bit in the beginning, right?&lt;/P&gt;</description>
    <pubDate>Thu, 30 Nov 2023 09:51:13 GMT</pubDate>
    <dc:creator>tks11111</dc:creator>
    <dc:date>2023-11-30T09:51:13Z</dc:date>
    <item>
      <title>LPC5528 Force USB1 as Full speed Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1764401#M54806</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the LPC5528 to run a project, and I need to support both high speed USB and full speed USB by using USB1. I saw there is a Forced FS bit in USB1-&amp;gt;DEVCMDSTAT that might be able to deal with it.&lt;/P&gt;&lt;P&gt;However, as I know, there are some differences between high speed USB and full speed USB such as the clock and the descriptor.&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;1. Do we need to do any configuration after setting the Forced FS bit to 1 if I want to force USB1 as a USB full speed device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Do we need to adjust any clock setting for it?&lt;/P&gt;&lt;P&gt;3. Is there any sample code that can be referenced? (toggle USB high speed and USB full speed in USB1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 01:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1764401#M54806</guid>
      <dc:creator>tks11111</dc:creator>
      <dc:date>2023-11-28T01:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 Force USB1 as Full speed Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1766376#M54837</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225107"&gt;@tks11111&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Setting the Force FS bit to 1 is the only thing that is required.&lt;/P&gt;
&lt;P&gt;Nothing else needs to be done. Clocks and other items are automatically configured by the HW in the correct mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 09:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1766376#M54837</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-11-30T09:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 Force USB1 as Full speed Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1766399#M54841</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Alice,&lt;/P&gt;&lt;P&gt;Thanks for the quick reply.&lt;/P&gt;&lt;P&gt;I had a quick question. If I want to toggle the USB1 between High Speed and Full Speed, I need to&lt;/P&gt;&lt;P&gt;call NVIC_SystemReset() and then toggle the Forced FS bit in the beginning, right?&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 09:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-Force-USB1-as-Full-speed-Device/m-p/1766399#M54841</guid>
      <dc:creator>tks11111</dc:creator>
      <dc:date>2023-11-30T09:51:13Z</dc:date>
    </item>
  </channel>
</rss>