<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC84x - how to read FRO frequency programmatically in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766280#M54831</link>
    <description>&lt;P&gt;Hello all,&lt;BR /&gt;In others LPC microcontroller I can determine the input frequency to the core and to the peripherials from running application.&lt;BR /&gt;But in the LPC84x series I don't know how.&lt;BR /&gt;Fro can be 30 MHz/24 MHz/18 MHz and I able to set it by set_fro_frequency API call.&lt;BR /&gt;But how to read it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 30 Nov 2023 07:47:25 GMT</pubDate>
    <dc:creator>pepoja</dc:creator>
    <dc:date>2023-11-30T07:47:25Z</dc:date>
    <item>
      <title>LPC84x - how to read FRO frequency programmatically</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766280#M54831</link>
      <description>&lt;P&gt;Hello all,&lt;BR /&gt;In others LPC microcontroller I can determine the input frequency to the core and to the peripherials from running application.&lt;BR /&gt;But in the LPC84x series I don't know how.&lt;BR /&gt;Fro can be 30 MHz/24 MHz/18 MHz and I able to set it by set_fro_frequency API call.&lt;BR /&gt;But how to read it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 07:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766280#M54831</guid>
      <dc:creator>pepoja</dc:creator>
      <dc:date>2023-11-30T07:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC84x - how to read FRO frequency programmatically</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766331#M54833</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, there is nowhere to read the clock for the core and a specific peripheral directly.&lt;/P&gt;
&lt;P&gt;Pls refer to section 8.5.1 Clock generation in UM11029.pdf, the application code can define the external crystal clock frequency or the clock frequency from CLKIN pin, then read the clock source mux and divider register to figure out the core clock frequency and peripheral clock frequency.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 08:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766331#M54833</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-11-30T08:46:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC84x - how to read FRO frequency programmatically</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766353#M54834</link>
      <description>&lt;P&gt;Thank You for your quick reply.&lt;/P&gt;&lt;P&gt;Yes, I know UM11029.pdf of course.&lt;BR /&gt;Due to the minimalization components count, I don't use external clock input/external crystal.&lt;/P&gt;&lt;P&gt;For my applications was FRO good solution. I was think....&lt;BR /&gt;All application timing is based on it. I must to know the input frequencu to clock generation engine.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Finnaly solution is:&lt;BR /&gt;Write desired FRO frequency by API call after each MCU reset.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;p.s. Why API doesn't include &lt;STRONG&gt;get_fro_frequency&lt;/STRONG&gt; also? It's a unbreakable problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Petetr&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 09:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-how-to-read-FRO-frequency-programmatically/m-p/1766353#M54834</guid>
      <dc:creator>pepoja</dc:creator>
      <dc:date>2023-11-30T09:06:12Z</dc:date>
    </item>
  </channel>
</rss>