<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to enable ETM In LPC5460X in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1764919#M54811</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;we try the above initializations and also initialization files also but it is not working.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PK_1114_0-1701175113442.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251887i16F9E30F63AFA15D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PK_1114_0-1701175113442.png" alt="PK_1114_0-1701175113442.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PK_1114_0-1701175113442.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;B Pavan Kumar&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 12:39:04 GMT</pubDate>
    <dc:creator>PK_1114</dc:creator>
    <dc:date>2023-11-28T12:39:04Z</dc:date>
    <item>
      <title>How to enable ETM In LPC5460X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763557#M54790</link>
      <description>&lt;P&gt;Hai,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the Ulink Pro debugger, I need to see execution profile using ETM in LPC1769 it is working fine while coming to the LPC54606 and LPC54608 hardware it is not working and showing no synchronization error. If possible please provide the test code for it.&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;B Pavan Kumar&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 25 Nov 2023 09:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763557#M54790</guid>
      <dc:creator>PK_1114</dc:creator>
      <dc:date>2023-11-25T09:56:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable ETM In LPC5460X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763703#M54793</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the ETM requires dedicated device and dedicated tools, we have not tested ETM module for LPC546xx.&lt;/P&gt;
&lt;P&gt;But we have tested the ETM module based on i.mxrt10xx, this is the link including the *.pdf and software.&lt;/P&gt;
&lt;P&gt;The LPC546xx has TRACEx pin, supports ETM.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/search?keyword=an12877&amp;amp;start=0" target="_blank"&gt;https://www.nxp.com/search?keyword=an12877&amp;amp;start=0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12877.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12877.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 27 Nov 2023 03:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763703#M54793</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-11-27T03:42:16Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable ETM In LPC5460X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763707#M54794</link>
      <description>Hi,&lt;BR /&gt;We already terminate the ETM Trace Pins (TraceCLK, Trace Data0, Trace Data1, Trace Data2, Trace Data 3) in Debugger Connector and we are using Ulink Pro Debugger for tracing and Keil UV5. But it is not working.&lt;BR /&gt;&lt;BR /&gt;Thank You,&lt;BR /&gt;B Pavan Kumar</description>
      <pubDate>Mon, 27 Nov 2023 03:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763707#M54794</guid>
      <dc:creator>PK_1114</dc:creator>
      <dc:date>2023-11-27T03:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable ETM In LPC5460X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763881#M54795</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that your own code includes the pin assignment and the trace clock divider.&lt;/P&gt;
&lt;P&gt;For example,the&amp;nbsp; PIO1_0 is assigned as Traceclk with func 5, for detail, pls refer to section Table 256. Type D I/O Control registers: FUNC values and pin functions in&amp;nbsp; UM10912.pdf&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in pin_mux.c, add the code:&lt;/P&gt;
&lt;P&gt;#defineIOCON_PIO_FUNC5 &lt;/P&gt;
&lt;P&gt;CLOCK_EnableClock(kCLOCK_Iocon);&lt;/P&gt;
&lt;P&gt;const uint32_t port1_pin0_config = (&lt;BR /&gt;IOCON_PIO_FUNC5 |&lt;BR /&gt;/* No addition pin function */&lt;BR /&gt;IOCON_PIO_MODE_INACT |&lt;BR /&gt;/* Input function is not inverted */&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;/* Enables digital function */&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;/* Input filter disabled */&lt;BR /&gt;IOCON_PIO_INPFILT_OFF |&lt;BR /&gt;/* Standard mode, output slew rate control is enabled */&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;/* Open drain is disabled */&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt;/* PORT1 PIN0 (coords: B13) is configured as traceclk*/&lt;BR /&gt;IOCON_PinMuxSet(IOCON, 1U, 0U, port1_pin0_config);&lt;/P&gt;
&lt;P&gt;//set the trace clock divider&lt;/P&gt;
&lt;P&gt;&amp;nbsp;CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 10U, false);&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 27 Nov 2023 08:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1763881#M54795</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-11-27T08:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable ETM In LPC5460X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1764919#M54811</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;we try the above initializations and also initialization files also but it is not working.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PK_1114_0-1701175113442.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251887i16F9E30F63AFA15D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PK_1114_0-1701175113442.png" alt="PK_1114_0-1701175113442.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PK_1114_0-1701175113442.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;B Pavan Kumar&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 12:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-enable-ETM-In-LPC5460X/m-p/1764919#M54811</guid>
      <dc:creator>PK_1114</dc:creator>
      <dc:date>2023-11-28T12:39:04Z</dc:date>
    </item>
  </channel>
</rss>