<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Firmware Update Using Secondary Bootloader</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762061#M54764</link>
    <description>&lt;P&gt;Hi All,&lt;BR /&gt;I am referring to AN12327 for Firmware update using the secondary bootloader.&lt;BR /&gt;In the startup file modifications which are mentioned "image header structure" needs to be added at the end of the vector table. I can see that the process and code are mentioned for iar and Keil but not for mcuxpresso ide. Can someone please help me to add the "Image header structure" after IVT for mcuxpresso ide&lt;/P&gt;</description>
    <pubDate>Wed, 22 Nov 2023 16:19:06 GMT</pubDate>
    <dc:creator>pranavitraj</dc:creator>
    <dc:date>2023-11-22T16:19:06Z</dc:date>
    <item>
      <title>Firmware Update Using Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762061#M54764</link>
      <description>&lt;P&gt;Hi All,&lt;BR /&gt;I am referring to AN12327 for Firmware update using the secondary bootloader.&lt;BR /&gt;In the startup file modifications which are mentioned "image header structure" needs to be added at the end of the vector table. I can see that the process and code are mentioned for iar and Keil but not for mcuxpresso ide. Can someone please help me to add the "Image header structure" after IVT for mcuxpresso ide&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 16:19:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762061#M54764</guid>
      <dc:creator>pranavitraj</dc:creator>
      <dc:date>2023-11-22T16:19:06Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update Using Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762244#M54767</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, are you referencing Table&amp;nbsp;2 Image header structure?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 00:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762244#M54767</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-11-23T00:33:42Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update Using Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762620#M54770</link>
      <description>&lt;P&gt;Hi Pavel,&lt;BR /&gt;&lt;BR /&gt;yes, i am referring to&amp;nbsp;&lt;SPAN&gt;Table&amp;nbsp;2 Image header structure.&lt;BR /&gt;and also the startup code modification, which mention&amp;nbsp;&lt;BR /&gt;"Put the image header at the end of vector table"&lt;BR /&gt;as shown in the below image.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pranavitraj_0-1700734814001.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251263i07C0820C84849675/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pranavitraj_0-1700734814001.png" alt="pranavitraj_0-1700734814001.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 10:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1762620#M54770</guid>
      <dc:creator>pranavitraj</dc:creator>
      <dc:date>2023-11-23T10:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update Using Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1764246#M54804</link>
      <description>&lt;P&gt;Hello, I confirmed with my team and the modification needs to be done as is mentioned in the AN.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1701110246348.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251679iB9DDC71A9EABB84A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1701110246348.png" alt="Pavel_Hernandez_0-1701110246348.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Mon, 27 Nov 2023 18:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/1764246#M54804</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-11-27T18:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Update Using Secondary Bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/2035987#M57603</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196430"&gt;@Pavel_Hernandez&lt;/a&gt;&amp;nbsp;can you please share how and where the function blHeader is defined.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jan 2025 05:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Firmware-Update-Using-Secondary-Bootloader/m-p/2035987#M57603</guid>
      <dc:creator>Pranav_Gupta</dc:creator>
      <dc:date>2025-01-30T05:29:21Z</dc:date>
    </item>
  </channel>
</rss>