<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PWM ISSUE - LPC 55s16 Microntroller in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1755945#M54687</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, pls download data sheet of lpc5516 and check it in pin description. For example, the PIO0-0 can function as CTIMER0_MAT0, which means that the pin can function to output PWM signal.&lt;/P&gt;
&lt;P&gt;PIO0_3 CTIMER0_MAT1&lt;/P&gt;
&lt;P&gt;PIO0_5 CTIMER3_MAT0&lt;/P&gt;
&lt;P&gt;PIO0_10 CTIMER2_MAT0&lt;/P&gt;
&lt;P&gt;.....&lt;/P&gt;
&lt;P&gt;In conclusion, all the CTIMERx_MATy pin can function as CTIMER PWM signal. In general, the MATCH0 register is used to configure the PWM period, so the CATIMERx_MAT0 is not used to output PWM. Of course, if you use the other match reg to control period, the MAT0 can be used to output PWM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1699839496009.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249483i4B06F5BF36818ADF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1699839496009.png" alt="xiangjun_rong_0-1699839496009.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1699839496009.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2)The SDK has example to have the CTIMER output PWM signal&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1699840108212.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249485iCEF0BB2F9335C272/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1699840108212.png" alt="xiangjun_rong_1-1699840108212.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_1-1699840108212.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the ctimer_PWM example, the PWM signal can output from PIO1_4 pin which multiplexed with CTIMER2_MAT1.&lt;/P&gt;
&lt;P&gt;The example uses CTIMER2 MAT2, we use the follow Macro&lt;/P&gt;
&lt;P&gt;#define CTIMER CTIMER2 /* Timer 2 */&lt;BR /&gt;#define CTIMER_MAT_OUT kCTIMER_Match_1 /* Match output 1 */&lt;/P&gt;
&lt;P&gt;In the pin_mux.c file, the following is defined:&lt;/P&gt;
&lt;P&gt;const uint32_t port1_pin4_config = (/* Pin is configured as CTIMER2_MAT1 */&lt;BR /&gt;IOCON_PIO_FUNC3 |&lt;BR /&gt;/* No addition pin function */&lt;BR /&gt;IOCON_PIO_MODE_INACT |&lt;BR /&gt;/* Standard mode, output slew rate control is enabled */&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;/* Input function is not inverted */&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;/* Enables digital function */&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;/* Open drain is disabled */&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt;/* PORT1 PIN4 (coords: 1) is configured as CTIMER2_MAT1 */&lt;BR /&gt;IOCON_PinMuxSet(IOCON, 1U, 4U, port1_pin4_config);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3)If you want to set the CTIMER2_MAT2 (pin PIO0_11) to output PWM. Pls try to use the code:&lt;/P&gt;
&lt;P&gt;#define IOCON_PIO_FUNC2 &lt;/P&gt;
&lt;P&gt;&amp;nbsp;const uint32_t port0_pin11_config = (/* Pin is configured as CTIMER2_MAT2 */&lt;BR /&gt;IOCON_PIO_FUNC2 |&lt;BR /&gt;/* No addition pin function */&lt;BR /&gt;IOCON_PIO_MODE_INACT |&lt;BR /&gt;/* Standard mode, output slew rate control is enabled */&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;/* Input function is not inverted */&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;/* Enables digital function */&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;/* Open drain is disabled */&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt;/* PORT0 PIN11 (coords: 1) is configured as CTIMER2_MAT2 */&lt;BR /&gt;IOCON_PinMuxSet(IOCON, 0U, 11U, port0_pin11_config);&lt;/P&gt;
&lt;P&gt;In the main.c&lt;/P&gt;
&lt;P&gt;#define CTIMER_MAT_OUT2 2&lt;BR /&gt;/* CTimer0 counter uses the AHB clock, some CTimer1 modules use the Aysnc clock */&lt;BR /&gt;srcClock_Hz = CTIMER_CLK_FREQ;&lt;/P&gt;
&lt;P&gt;PRINTF("CTimer example to generate a PWM signal\r\n");&lt;/P&gt;
&lt;P&gt;CTIMER_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;timerClock = srcClock_Hz / (config.prescale + 1);&lt;/P&gt;
&lt;P&gt;CTIMER_Init(CTIMER, &amp;amp;config);&lt;/P&gt;
&lt;P&gt;/* Get the PWM period match value and pulse width match value of 20Khz PWM signal with 20% dutycycle */&lt;BR /&gt;CTIMER_GetPwmPeriodValue(20000, 20, timerClock);&lt;BR /&gt;CTIMER_SetupPwmPeriod(CTIMER, CTIMER_MAT_PWM_PERIOD_CHANNEL, CTIMER_MAT_OUT, g_pwmPeriod, g_pulsePeriod, false);&lt;BR /&gt;CTIMER_SetupPwmPeriod(CTIMER, CTIMER_MAT_PWM_PERIOD_CHANNEL, CTIMER_MAT_OUT2, g_pwmPeriod, g_pulsePeriod, false);&lt;BR /&gt;CTIMER_StartTimer(CTIMER);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pls have a try.&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 13 Nov 2023 02:14:41 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-11-13T02:14:41Z</dc:date>
    <item>
      <title>PWM ISSUE - LPC 55s16 Microntroller</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1755831#M54684</link>
      <description>&lt;P&gt;I configured PWM pulse port-1 pin-4 its working ,but,&lt;/P&gt;&lt;P&gt;when i try to generate PWM pulse in&lt;STRONG&gt; port-0 pin-31 its NOT working.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;please update me if any changes to my below configuration&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN&gt;int&lt;/SPAN&gt; &lt;SPAN&gt;main&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ctimer_config_t&lt;/SPAN&gt;&lt;SPAN&gt; config;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt; srcClock_Hz;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt; timerClock;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* &lt;/SPAN&gt;&lt;SPAN&gt;Init&lt;/SPAN&gt;&lt;SPAN&gt; hardware*/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* set BOD VBAT level to 1.65V */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;POWER_SetBodVbatLevel(&lt;/SPAN&gt;&lt;SPAN&gt;kPOWER_BodVbatLevel1650mv&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;kPOWER_BodHystLevel50mv&lt;/SPAN&gt;&lt;SPAN&gt;, false);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* attach 12 MHz clock to FLEXCOMM0 (debug console) */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* Use 12 MHz clock for some of the &lt;/SPAN&gt;&lt;SPAN&gt;Ctimers&lt;/SPAN&gt;&lt;SPAN&gt; */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CLOCK_AttachClk(&lt;/SPAN&gt;&lt;SPAN&gt;kFRO_HF_to_CTIMER2&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BOARD_InitBootPins();&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BOARD_InitBootClocks();&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BOARD_InitDebugConsole();&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* CTimer0 counter uses the AHB clock, some CTimer1 modules use the &lt;/SPAN&gt;&lt;SPAN&gt;Aysnc&lt;/SPAN&gt;&lt;SPAN&gt; clock */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;srcClock_Hz = CTIMER_CLK_FREQ;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PRINTF(&lt;/SPAN&gt;&lt;SPAN&gt;"CTimer example to generate a PWM signal\r\n"&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PRINTF(&lt;/SPAN&gt;&lt;SPAN&gt;"This example uses interrupts to update the PWM duty cycle\r\n"&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CTIMER_GetDefaultConfig(&amp;amp;config);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;timerClock = srcClock_Hz / (config.&lt;/SPAN&gt;&lt;SPAN&gt;prescale&lt;/SPAN&gt;&lt;SPAN&gt; + 1);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CTIMER_Init(CTIMER, &amp;amp;config);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CTIMER_RegisterCallBack(CTIMER, &amp;amp;ctimer_callback[0], &lt;/SPAN&gt;&lt;SPAN&gt;kCTIMER_SingleCallback&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/* Get the PWM period match value and pulse width match value of 2Khz PWM signal */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CTIMER_GetPwmPeriodValue(20, dutyCycle, timerClock);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CTIMER_SetupPwmPeriod(CTIMER, CTIMER_MAT_PWM_PERIOD_CHANNEL, CTIMER_MAT_OUT, g_pwmPeriod, g_pulsePeriod, true);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CTIMER_StartTimer(CTIMER);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;while&lt;/SPAN&gt;&lt;SPAN&gt; (1)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 11 Nov 2023 07:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1755831#M54684</guid>
      <dc:creator>Arularasan</dc:creator>
      <dc:date>2023-11-11T07:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: PWM ISSUE - LPC 55s16 Microntroller</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1755945#M54687</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, pls download data sheet of lpc5516 and check it in pin description. For example, the PIO0-0 can function as CTIMER0_MAT0, which means that the pin can function to output PWM signal.&lt;/P&gt;
&lt;P&gt;PIO0_3 CTIMER0_MAT1&lt;/P&gt;
&lt;P&gt;PIO0_5 CTIMER3_MAT0&lt;/P&gt;
&lt;P&gt;PIO0_10 CTIMER2_MAT0&lt;/P&gt;
&lt;P&gt;.....&lt;/P&gt;
&lt;P&gt;In conclusion, all the CTIMERx_MATy pin can function as CTIMER PWM signal. In general, the MATCH0 register is used to configure the PWM period, so the CATIMERx_MAT0 is not used to output PWM. Of course, if you use the other match reg to control period, the MAT0 can be used to output PWM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1699839496009.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249483i4B06F5BF36818ADF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1699839496009.png" alt="xiangjun_rong_0-1699839496009.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1699839496009.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2)The SDK has example to have the CTIMER output PWM signal&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1699840108212.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249485iCEF0BB2F9335C272/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1699840108212.png" alt="xiangjun_rong_1-1699840108212.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_1-1699840108212.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the ctimer_PWM example, the PWM signal can output from PIO1_4 pin which multiplexed with CTIMER2_MAT1.&lt;/P&gt;
&lt;P&gt;The example uses CTIMER2 MAT2, we use the follow Macro&lt;/P&gt;
&lt;P&gt;#define CTIMER CTIMER2 /* Timer 2 */&lt;BR /&gt;#define CTIMER_MAT_OUT kCTIMER_Match_1 /* Match output 1 */&lt;/P&gt;
&lt;P&gt;In the pin_mux.c file, the following is defined:&lt;/P&gt;
&lt;P&gt;const uint32_t port1_pin4_config = (/* Pin is configured as CTIMER2_MAT1 */&lt;BR /&gt;IOCON_PIO_FUNC3 |&lt;BR /&gt;/* No addition pin function */&lt;BR /&gt;IOCON_PIO_MODE_INACT |&lt;BR /&gt;/* Standard mode, output slew rate control is enabled */&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;/* Input function is not inverted */&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;/* Enables digital function */&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;/* Open drain is disabled */&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt;/* PORT1 PIN4 (coords: 1) is configured as CTIMER2_MAT1 */&lt;BR /&gt;IOCON_PinMuxSet(IOCON, 1U, 4U, port1_pin4_config);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3)If you want to set the CTIMER2_MAT2 (pin PIO0_11) to output PWM. Pls try to use the code:&lt;/P&gt;
&lt;P&gt;#define IOCON_PIO_FUNC2 &lt;/P&gt;
&lt;P&gt;&amp;nbsp;const uint32_t port0_pin11_config = (/* Pin is configured as CTIMER2_MAT2 */&lt;BR /&gt;IOCON_PIO_FUNC2 |&lt;BR /&gt;/* No addition pin function */&lt;BR /&gt;IOCON_PIO_MODE_INACT |&lt;BR /&gt;/* Standard mode, output slew rate control is enabled */&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;/* Input function is not inverted */&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;/* Enables digital function */&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;/* Open drain is disabled */&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt;/* PORT0 PIN11 (coords: 1) is configured as CTIMER2_MAT2 */&lt;BR /&gt;IOCON_PinMuxSet(IOCON, 0U, 11U, port0_pin11_config);&lt;/P&gt;
&lt;P&gt;In the main.c&lt;/P&gt;
&lt;P&gt;#define CTIMER_MAT_OUT2 2&lt;BR /&gt;/* CTimer0 counter uses the AHB clock, some CTimer1 modules use the Aysnc clock */&lt;BR /&gt;srcClock_Hz = CTIMER_CLK_FREQ;&lt;/P&gt;
&lt;P&gt;PRINTF("CTimer example to generate a PWM signal\r\n");&lt;/P&gt;
&lt;P&gt;CTIMER_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;timerClock = srcClock_Hz / (config.prescale + 1);&lt;/P&gt;
&lt;P&gt;CTIMER_Init(CTIMER, &amp;amp;config);&lt;/P&gt;
&lt;P&gt;/* Get the PWM period match value and pulse width match value of 20Khz PWM signal with 20% dutycycle */&lt;BR /&gt;CTIMER_GetPwmPeriodValue(20000, 20, timerClock);&lt;BR /&gt;CTIMER_SetupPwmPeriod(CTIMER, CTIMER_MAT_PWM_PERIOD_CHANNEL, CTIMER_MAT_OUT, g_pwmPeriod, g_pulsePeriod, false);&lt;BR /&gt;CTIMER_SetupPwmPeriod(CTIMER, CTIMER_MAT_PWM_PERIOD_CHANNEL, CTIMER_MAT_OUT2, g_pwmPeriod, g_pulsePeriod, false);&lt;BR /&gt;CTIMER_StartTimer(CTIMER);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pls have a try.&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 02:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1755945#M54687</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-11-13T02:14:41Z</dc:date>
    </item>
    <item>
      <title>Re: PWM ISSUE - LPC 55s16 Microntroller</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1895708#M56325</link>
      <description>&lt;P&gt;Dear Xiangjun,&lt;/P&gt;&lt;P&gt;I try to use the simple_pwm_interrupt demo to control the rgb led, how can I control the led on delay by the pwm cycle count insteal of the function bsp_delay_time.&lt;/P&gt;&lt;P&gt;Best Wish!&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 06:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1895708#M56325</guid>
      <dc:creator>JJ3</dc:creator>
      <dc:date>2024-06-28T06:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: PWM ISSUE - LPC 55s16 Microntroller</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1901058#M56404</link>
      <description>&lt;P&gt;This issue has bother me for a week. finally find the working solution. Thanks.&lt;/P&gt;</description>
      <pubDate>Sun, 07 Jul 2024 08:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-ISSUE-LPC-55s16-Microntroller/m-p/1901058#M56404</guid>
      <dc:creator>putavi</dc:creator>
      <dc:date>2024-07-07T08:20:52Z</dc:date>
    </item>
  </channel>
</rss>