<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックDeep Sleep Mode in LPC55S69</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-Sleep-Mode-in-LPC55S69/m-p/1751951#M54630</link>
    <description>&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;I'm working on Deep sleep mode in LPC55S69 EVK,I have referred the AN13265 and the user manual .I have also checked the SDK example of uart and power manage .&lt;/P&gt;&lt;P&gt;Board used :&lt;STRONG&gt;LPC55S69.&lt;BR /&gt;&lt;/STRONG&gt;SDK used :power_manager_lpc and&amp;nbsp;usart_wakeup_deepsleep.&lt;BR /&gt;&lt;BR /&gt;PROBLEM :-&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;How do I verify that the system has gone into deep sleep mode ??Similarly how to verify that the system has woken up from sleep?&lt;/LI&gt;&lt;LI&gt;By default does all the peripheral clock be deactivated avoiding to the user manual??&lt;/LI&gt;&lt;LI&gt;Should I configure the clock once again after waking up from the deep sleep??&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Is there any procedure I need to follow for configuring the main clock ??&lt;/LI&gt;&lt;LI&gt;In case I turn on the deep sleep mode and I don't give any wake-up interrupt ,how do i wake up the system ??&lt;/LI&gt;&lt;LI&gt;Any suggestion on how i should move forward .I need to make sure the module is in deep sleep mode only when a peripheral such as FLEXCOMM and gpio enables interrupt ,the system needs to wake up.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you and regards&amp;nbsp;&lt;BR /&gt;&lt;SPAN&gt;UJWAL KUMAR N L&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171674"&gt;@Juan-Rodarte&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/49"&gt;@jesseg&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;#lpc55s69 #deepsleepmode&lt;/P&gt;</description>
    <pubDate>Fri, 03 Nov 2023 12:00:12 GMT</pubDate>
    <dc:creator>ujwal_kumar_N_L</dc:creator>
    <dc:date>2023-11-03T12:00:12Z</dc:date>
    <item>
      <title>Deep Sleep Mode in LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-Sleep-Mode-in-LPC55S69/m-p/1751951#M54630</link>
      <description>&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;I'm working on Deep sleep mode in LPC55S69 EVK,I have referred the AN13265 and the user manual .I have also checked the SDK example of uart and power manage .&lt;/P&gt;&lt;P&gt;Board used :&lt;STRONG&gt;LPC55S69.&lt;BR /&gt;&lt;/STRONG&gt;SDK used :power_manager_lpc and&amp;nbsp;usart_wakeup_deepsleep.&lt;BR /&gt;&lt;BR /&gt;PROBLEM :-&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;How do I verify that the system has gone into deep sleep mode ??Similarly how to verify that the system has woken up from sleep?&lt;/LI&gt;&lt;LI&gt;By default does all the peripheral clock be deactivated avoiding to the user manual??&lt;/LI&gt;&lt;LI&gt;Should I configure the clock once again after waking up from the deep sleep??&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Is there any procedure I need to follow for configuring the main clock ??&lt;/LI&gt;&lt;LI&gt;In case I turn on the deep sleep mode and I don't give any wake-up interrupt ,how do i wake up the system ??&lt;/LI&gt;&lt;LI&gt;Any suggestion on how i should move forward .I need to make sure the module is in deep sleep mode only when a peripheral such as FLEXCOMM and gpio enables interrupt ,the system needs to wake up.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you and regards&amp;nbsp;&lt;BR /&gt;&lt;SPAN&gt;UJWAL KUMAR N L&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171674"&gt;@Juan-Rodarte&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/49"&gt;@jesseg&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;#lpc55s69 #deepsleepmode&lt;/P&gt;</description>
      <pubDate>Fri, 03 Nov 2023 12:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-Sleep-Mode-in-LPC55S69/m-p/1751951#M54630</guid>
      <dc:creator>ujwal_kumar_N_L</dc:creator>
      <dc:date>2023-11-03T12:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: Deep Sleep Mode in LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-Sleep-Mode-in-LPC55S69/m-p/1752592#M54642</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1.How do I verify that the system has gone into deep sleep mode ??Similarly how to verify that the system has woken up from sleep?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;You can toggle a LED in the main loop with a delay() function. After you enter deep sleep mode, the led does not toggle. After waking-up, the LED continues to toggle.&lt;/P&gt;
&lt;P&gt;2.By default does all the peripheral clock be deactivated avoiding to the user manual?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Yes, the cpu main clock and peripherals clock are disabled in default in deep sleep mode.&lt;/P&gt;
&lt;P&gt;3.Should I configure the clock once again after waking up from the deep sleep??&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;After waking-up, the internal 12MHz clock will be the default clock.&lt;/P&gt;
&lt;P&gt;4.Is there any procedure I need to follow for configuring the main clock ??&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;You can configure the main clock when the chip is in active mode.&lt;/P&gt;
&lt;P&gt;5.In case I turn on the deep sleep mode and I don't give any wake-up interrupt ,how do i wake up the system ??&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;The chip will remain in deep sleep mode forever, in other words, you have to wake-up with interrupt event.&lt;/P&gt;
&lt;P&gt;6.Any suggestion on how i should move forward .I need to make sure the module is in deep sleep mode only when a peripheral such as FLEXCOMM and gpio enables interrupt ,the system needs to wake up.&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;There is an example in SDK package:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1699256444390.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/248570i21D28DB55A6264D6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1699256444390.png" alt="xiangjun_rong_0-1699256444390.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1699256444390.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 07:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-Sleep-Mode-in-LPC55S69/m-p/1752592#M54642</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-11-06T07:41:55Z</dc:date>
    </item>
  </channel>
</rss>