<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックExternal debugger SWD OR J-TAG</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-debugger-SWD-OR-J-TAG/m-p/1748636#M54570</link>
    <description>&lt;P&gt;Hi Community ,&lt;/P&gt;&lt;P&gt;Im working on the debugger ofLPC55S69 ,trying to use the microcontroller and program it with external Debugger .&lt;/P&gt;&lt;P&gt;Board :LPC55S69&lt;/P&gt;&lt;P&gt;Debugging using SWD.&lt;BR /&gt;&lt;BR /&gt;PROBLEM:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Can we use the external debugger to dump the code to the microcontroller ?(Using only SWD not JLINK).&lt;/LI&gt;&lt;LI&gt;Can we only use&amp;nbsp; SWCLK,SWDIO and SWO instead of the 10 pin P7 SWD .Only utilizing these 3 pins and debugging it module?&lt;/LI&gt;&lt;LI&gt;Best external debugger for dumping the code .Suggestions.&lt;/LI&gt;&lt;LI&gt;Steps or material regarding the above Debugging.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank and Regards&amp;nbsp;&lt;BR /&gt;UJWAL KUMAR N L&lt;/P&gt;</description>
    <pubDate>Mon, 30 Oct 2023 10:12:31 GMT</pubDate>
    <dc:creator>ujwal_kumar_N_L</dc:creator>
    <dc:date>2023-10-30T10:12:31Z</dc:date>
    <item>
      <title>External debugger SWD OR J-TAG</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-debugger-SWD-OR-J-TAG/m-p/1748636#M54570</link>
      <description>&lt;P&gt;Hi Community ,&lt;/P&gt;&lt;P&gt;Im working on the debugger ofLPC55S69 ,trying to use the microcontroller and program it with external Debugger .&lt;/P&gt;&lt;P&gt;Board :LPC55S69&lt;/P&gt;&lt;P&gt;Debugging using SWD.&lt;BR /&gt;&lt;BR /&gt;PROBLEM:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Can we use the external debugger to dump the code to the microcontroller ?(Using only SWD not JLINK).&lt;/LI&gt;&lt;LI&gt;Can we only use&amp;nbsp; SWCLK,SWDIO and SWO instead of the 10 pin P7 SWD .Only utilizing these 3 pins and debugging it module?&lt;/LI&gt;&lt;LI&gt;Best external debugger for dumping the code .Suggestions.&lt;/LI&gt;&lt;LI&gt;Steps or material regarding the above Debugging.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank and Regards&amp;nbsp;&lt;BR /&gt;UJWAL KUMAR N L&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 10:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-debugger-SWD-OR-J-TAG/m-p/1748636#M54570</guid>
      <dc:creator>ujwal_kumar_N_L</dc:creator>
      <dc:date>2023-10-30T10:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: External debugger SWD OR J-TAG</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-debugger-SWD-OR-J-TAG/m-p/1748652#M54572</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221323"&gt;@ujwal_kumar_N_L&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;1. If you mean with 'dump the code to the microcontroller' the programming and flashing of it, then yes: you can use SWD for this. You don't have to use a J-Link, you can use any other debug probe supporting the LPC55S69, e.g. MCU-Link (Pro) or P&amp;amp;E Multilink.&lt;/P&gt;&lt;P&gt;2. You need SWCKL, SWDIO and GND. SWO is a trace pin, see &lt;A href="https://mcuoneclipse.com/2021/05/22/swo-with-arm-cortex-m33/" target="_blank" rel="noopener"&gt;https://mcuoneclipse.com/2021/05/22/swo-with-arm-cortex-m33/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;3. Use a J-Link, or program the J-Link firmware on the board. Or use the NXP MCU-Link Pro or non-pro, or use a P&amp;amp;E Multilink. Choice depends on your needs and budget available.&lt;/P&gt;&lt;P&gt;4. &lt;A href="https://mcuoneclipse.com/2019/05/18/internal-and-external-debug-options-for-the-nxp-lpc55s69-evk-board/" target="_blank" rel="noopener"&gt;https://mcuoneclipse.com/2019/05/18/internal-and-external-debug-options-for-the-nxp-lpc55s69-evk-board/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 10:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-debugger-SWD-OR-J-TAG/m-p/1748652#M54572</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-10-30T10:41:54Z</dc:date>
    </item>
  </channel>
</rss>