<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Porting SE05x evaluation board SKD example for LPC55S69 on LPC55S06</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Porting-SE05x-evaluation-board-SKD-example-for-LPC55S69-on/m-p/1739380#M54392</link>
    <description>&lt;P&gt;Hi guys! I'm trying to make some porting for running SE05X example from se_hostlib SDK for LPC55S69 on LPC55S06. I'm stuck on the configuration of the board directory which contain the board-clock_config-pin_mux library (and header).&lt;/P&gt;&lt;P&gt;The documentation is a bit poor on this matter, has anyone already done something or can give me some guidance? Thank you!&lt;/P&gt;</description>
    <pubDate>Fri, 13 Oct 2023 09:14:09 GMT</pubDate>
    <dc:creator>WorkerEmbedded</dc:creator>
    <dc:date>2023-10-13T09:14:09Z</dc:date>
    <item>
      <title>Porting SE05x evaluation board SKD example for LPC55S69 on LPC55S06</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Porting-SE05x-evaluation-board-SKD-example-for-LPC55S69-on/m-p/1739380#M54392</link>
      <description>&lt;P&gt;Hi guys! I'm trying to make some porting for running SE05X example from se_hostlib SDK for LPC55S69 on LPC55S06. I'm stuck on the configuration of the board directory which contain the board-clock_config-pin_mux library (and header).&lt;/P&gt;&lt;P&gt;The documentation is a bit poor on this matter, has anyone already done something or can give me some guidance? Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 13 Oct 2023 09:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Porting-SE05x-evaluation-board-SKD-example-for-LPC55S69-on/m-p/1739380#M54392</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2023-10-13T09:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: Porting SE05x evaluation board SKD example for LPC55S69 on LPC55S06</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Porting-SE05x-evaluation-board-SKD-example-for-LPC55S69-on/m-p/1740813#M54434</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Frankly speaking, I am not familiar with SE05x, but I am familiar with LPC55S06.&lt;/P&gt;
&lt;P&gt;I suppose that the LPC55S06 uses I2C as a master to communicate with SE05x, pls check the schematics and know the I2C interface port and pins.&lt;/P&gt;
&lt;P&gt;The LPC55S06 has SDK package, after you get the I2C port and pins, you can use the I2C example as the following fig, then modify the pin_mux.c to change the pins of I2C, and change the I2C port in *_master.c with the code like:&lt;/P&gt;
&lt;P&gt;#define EXAMPLE_I2C_MASTER_BASE (I2C3_BASE)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1697510494091.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/245383i436CAFC729E01581/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1697510494091.png" alt="xiangjun_rong_0-1697510494091.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This is the SE05x community thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Secure-Authentication/bd-p/secure-authentication" target="_blank"&gt;https://community.nxp.com/t5/Secure-Authentication/bd-p/secure-authentication&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Oct 2023 02:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Porting-SE05x-evaluation-board-SKD-example-for-LPC55S69-on/m-p/1740813#M54434</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-10-17T02:47:54Z</dc:date>
    </item>
  </channel>
</rss>