<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC5516JVE59 boot mode and CAN interface in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1733224#M54265</link>
    <description>&lt;P&gt;Any comments from NXP??&lt;/P&gt;</description>
    <pubDate>Tue, 03 Oct 2023 15:30:31 GMT</pubDate>
    <dc:creator>HPT_Dave</dc:creator>
    <dc:date>2023-10-03T15:30:31Z</dc:date>
    <item>
      <title>LPC5516JVE59 boot mode and CAN interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1730769#M54232</link>
      <description>&lt;P&gt;I need a little help understanding how to use the the boot mode and CAN interface (CAN_TX) when both options share the same pin (C6) on the LPC5516JVE59 BGA package. As I understand the documentation, on reset, the processor looks to the boot mode pin (C6 for the LPC5516JVE59) to determine passive or ISP BOOT. I'm planning on using the passive boot mode for my design which requires (?) an external pullup resistor. Once the image is found in the internal Flash, my program will be able to configure the pin to be the CAN_TX option. The confusion I have is the the external pullup will still be present on the CAN_TX pin. Won't this pullup create problems for the the CAN_TX line to perform correctly?&lt;/P&gt;&lt;P&gt;Thanks for the help,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 20:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1730769#M54232</guid>
      <dc:creator>HPT_Dave</dc:creator>
      <dc:date>2023-09-27T20:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516JVE59 boot mode and CAN interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1733224#M54265</link>
      <description>&lt;P&gt;Any comments from NXP??&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 15:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1733224#M54265</guid>
      <dc:creator>HPT_Dave</dc:creator>
      <dc:date>2023-10-03T15:30:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516JVE59 boot mode and CAN interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1735177#M54288</link>
      <description>&lt;P&gt;Hi&amp;nbsp;HPT_Dave&amp;nbsp;&lt;/P&gt;
&lt;P&gt;LPC5516 doesn't supprot CAN ISP in Boot ROM. It supports USB, SPI, I2C ISP only.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1696685755685.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/243959i5FB46688FA711780/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1696685755685.png" alt="ZhangJennie_0-1696685755685.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_0-1696685755685.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If CAN boot is must, you need to implement your own secondary CAN bootloader with referring&amp;nbsp;&lt;/P&gt;
&lt;H3 class="item-title"&gt;&lt;FONT size="3"&gt;&lt;A id="relatedDocsClickPDF_20" class="dtmcustomrulelink" href="https://www.nxp.com/docs/en/application-note/AN12327.pdf" target="_blank" rel="noopener" data-dtmaction="Documentation Section - Results Link Click" data-dtmsubaction="AN12327 - Firmware Update Using Secondary Bootloader - NXP - Application Note - English"&gt;&lt;SPAN&gt;AN12327 - Firmware Update Using Secondary Bootloader&lt;/SPAN&gt;&lt;/A&gt;&lt;/FONT&gt;&lt;/H3&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12327SW.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note-software/AN12327SW.zip&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;and CAN driver demo code unser MCUXpresso SDK folder.&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 07 Oct 2023 13:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516JVE59-boot-mode-and-CAN-interface/m-p/1735177#M54288</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-10-07T13:40:41Z</dc:date>
    </item>
  </channel>
</rss>