<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1732370#M54256</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;can you help check if the&amp;nbsp;&lt;SPAN&gt;Secure Provisioning tool&amp;nbsp;works when&amp;nbsp;&lt;/SPAN&gt;USB1 is&amp;nbsp; configured as full speed mode?&lt;/P&gt;&lt;P&gt;also,&amp;nbsp; please provide instructions on how to configure the USB full speed mode in&amp;nbsp;&lt;SPAN&gt;Provisioning tool.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 01 Oct 2023 23:21:27 GMT</pubDate>
    <dc:creator>jasonz2021</dc:creator>
    <dc:date>2023-10-01T23:21:27Z</dc:date>
    <item>
      <title>Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1725883#M54139</link>
      <description>&lt;P&gt;I have been able to program an LPCXpress 55S28 board using Flash Magic through the UART, but unable to do so through USB1 (high speed).&lt;/P&gt;&lt;P&gt;I can see the USB interface appear in Flash Magic. I can read the signature. But I can't program it. The error is&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;LPC55S28 (USB, LPC5500) Operation Failed. (programming - failed to send data to the device)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have tried it with both Flash Magic 13.50 and 13.61, both unsuccessful.&lt;/P&gt;&lt;P&gt;This person seems to have encountered this too, several years ago, without resolution:&lt;/P&gt;&lt;P&gt;&lt;A href="https://forum.flashmagictool.com/index.php?topic=6537.0" target="_blank" rel="noopener"&gt;LPC55S28 (USB, LPC5500) Operation failed&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Another person has reported a similar error with LPC55S69:&lt;/P&gt;&lt;P&gt;&lt;A href="https://forum.flashmagictool.com/index.php?topic=11201.0" target="_blank"&gt;LPC55S69 Not Programming through USB&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 05:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1725883#M54139</guid>
      <dc:creator>craigmcqueenir</dc:creator>
      <dc:date>2023-09-21T05:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1728404#M54191</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/140851"&gt;@craigmcqueenir&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How about program a simple led_blinky image? If still failed, take a screenshot about your steps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 01:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1728404#M54191</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-09-25T01:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1729342#M54211</link>
      <description>&lt;P&gt;As I said, I am able to program my application into the processor using Flash Magic via UART. But not via USB. So I don't think I need to try the led_blinky image, since I have verified my own application is fine via UART.&lt;/P&gt;&lt;P&gt;I will endeavour to provide screen shots as soon as I can collect them.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 04:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1729342#M54211</guid>
      <dc:creator>craigmcqueenir</dc:creator>
      <dc:date>2023-09-26T04:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1729555#M54215</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/140851"&gt;@craigmcqueenir&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I tested on my side, yes, there is issue with Flash Magic.&lt;/P&gt;
&lt;P&gt;You can use MCUXpresso Secure Provisioning tool to program, I took a video about steps, please see my attachment.&lt;/P&gt;
&lt;P&gt;Download tool from:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING&lt;/A&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 08:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1729555#M54215</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-09-26T08:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1730163#M54223</link>
      <description>&lt;P&gt;Thanks. I haven't tried it yet, but I see it uses &lt;STRONG&gt;blhost&lt;/STRONG&gt; to do the writes. I have successfully used &lt;STRONG&gt;blhost&lt;/STRONG&gt; to write the Flash of the LPCXpresso 55S28 board via its USB1.&lt;/P&gt;&lt;P&gt;It would still be good if the problem with Flash Magic could be fixed.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 05:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1730163#M54223</guid>
      <dc:creator>craigmcqueenir</dc:creator>
      <dc:date>2023-09-27T05:53:44Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program LPCXpresso 55S28 via USB1 HS with Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1732370#M54256</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;can you help check if the&amp;nbsp;&lt;SPAN&gt;Secure Provisioning tool&amp;nbsp;works when&amp;nbsp;&lt;/SPAN&gt;USB1 is&amp;nbsp; configured as full speed mode?&lt;/P&gt;&lt;P&gt;also,&amp;nbsp; please provide instructions on how to configure the USB full speed mode in&amp;nbsp;&lt;SPAN&gt;Provisioning tool.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 01 Oct 2023 23:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unable-to-program-LPCXpresso-55S28-via-USB1-HS-with-Flash-Magic/m-p/1732370#M54256</guid>
      <dc:creator>jasonz2021</dc:creator>
      <dc:date>2023-10-01T23:21:27Z</dc:date>
    </item>
  </channel>
</rss>