<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S69 Dual Core From Flash in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Dual-Core-From-Flash/m-p/1729758#M54218</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am currently looking into running the LPC55S69 microcontroller on both cores.&amp;nbsp;&lt;/P&gt;&lt;P&gt;From following the SDK examples I see that the second core is run entirely from RAM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to have both images running from flash memory instead?&lt;/P&gt;&lt;P&gt;KR,&lt;/P&gt;&lt;P&gt;Blair&lt;/P&gt;</description>
    <pubDate>Tue, 26 Sep 2023 12:50:49 GMT</pubDate>
    <dc:creator>bs_123</dc:creator>
    <dc:date>2023-09-26T12:50:49Z</dc:date>
    <item>
      <title>LPC55S69 Dual Core From Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Dual-Core-From-Flash/m-p/1729758#M54218</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am currently looking into running the LPC55S69 microcontroller on both cores.&amp;nbsp;&lt;/P&gt;&lt;P&gt;From following the SDK examples I see that the second core is run entirely from RAM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to have both images running from flash memory instead?&lt;/P&gt;&lt;P&gt;KR,&lt;/P&gt;&lt;P&gt;Blair&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 12:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Dual-Core-From-Flash/m-p/1729758#M54218</guid>
      <dc:creator>bs_123</dc:creator>
      <dc:date>2023-09-26T12:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 Dual Core From Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Dual-Core-From-Flash/m-p/1731434#M54239</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221977"&gt;@bs_123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The next post will provide you the information you are looking for:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-Dual-Core-Best-Practice/td-p/946035" target="_self"&gt;LPC55S6x: Dual Core Best Practice&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope it helps.&lt;/P&gt;
&lt;P&gt;Best Regard, Miguel.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 17:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Dual-Core-From-Flash/m-p/1731434#M54239</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-09-28T17:36:51Z</dc:date>
    </item>
  </channel>
</rss>