<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC553x: Using internal LDO instead of internal DCDC converter in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728441#M54192</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Yes, the LPC5536/LPC55S36 has both internal DC/DC converter and LDO for VDD_CORE power supply, if you use internal LDO, it is okay to just connect a 4.7uF cap to the VDD_CORE pin.&lt;/P&gt;
&lt;P&gt;You can connect 3.3V power supply to the VDD_MIAN and VDD_MAIN_PWR pins.&lt;/P&gt;
&lt;P&gt;The remark "The internal LDO allows the MCU to use an external regulation element" just means that the 3.3V power supply which is connected to VDD_MIAN and VDD_MAIN_PWR can be from external DC/DC converter or external LDO.&lt;/P&gt;
&lt;P&gt;For example, you have 5V power supply, there is an external Buck DC/DC converter which convert 5V to 3.3V, the 3.3V can power the VDD_MIAN and VDD_MAIN_PWR pins.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 25 Sep 2023 02:12:57 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-09-25T02:12:57Z</dc:date>
    <item>
      <title>LPC553x: Using internal LDO instead of internal DCDC converter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728132#M54186</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I see that the LPC553x series include an internal LDO which can be used instead of the internal DCDC converter. At least this is my understanding from reading &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN13528.pdf" target="_self"&gt;AN13528&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Is it correct that to use the internal LDO, I just have to drop the inductor (which is connected to LX in order to use the internal DCDC converter) so that I end up with this configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielholala_0-1695396449458.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/242301i7F9204EE265118A1/image-size/large?v=v2&amp;amp;px=999" role="button" title="danielholala_0-1695396449458.png" alt="danielholala_0-1695396449458.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now I have these question:&lt;/P&gt;&lt;P&gt;Do I just have to connect VDD_MAIN to 3.3V to get the MCU powered? I'm asking because&amp;nbsp;the application note states "The internal LDO allows the MCU to use an external regulation element". What does that mean? Which "external regulation element" do I have to add and where? Is that a requirement to use the internal LDO?&lt;/P&gt;&lt;P&gt;Further, Do I have to "enable" the internal LDO?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 15:31:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728132#M54186</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-09-22T15:31:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: Using internal LDO instead of internal DCDC converter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728441#M54192</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Yes, the LPC5536/LPC55S36 has both internal DC/DC converter and LDO for VDD_CORE power supply, if you use internal LDO, it is okay to just connect a 4.7uF cap to the VDD_CORE pin.&lt;/P&gt;
&lt;P&gt;You can connect 3.3V power supply to the VDD_MIAN and VDD_MAIN_PWR pins.&lt;/P&gt;
&lt;P&gt;The remark "The internal LDO allows the MCU to use an external regulation element" just means that the 3.3V power supply which is connected to VDD_MIAN and VDD_MAIN_PWR can be from external DC/DC converter or external LDO.&lt;/P&gt;
&lt;P&gt;For example, you have 5V power supply, there is an external Buck DC/DC converter which convert 5V to 3.3V, the 3.3V can power the VDD_MIAN and VDD_MAIN_PWR pins.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 02:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728441#M54192</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-25T02:12:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: Using internal LDO instead of internal DCDC converter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728644#M54199</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for your reply. That clears thing up. I understand that I do not have to enable the internal LDO. It is automatically active when the DCDC converter output (LX pin) is not connected to VDD_CORE via an inductor.&lt;/P&gt;&lt;P&gt;Regarding&amp;nbsp;the remark "&lt;EM&gt;The internal LDO allows the MCU to use an external regulation element&lt;/EM&gt;" you wrote that this means that the 3.3V power supply which is connected to VDD_MIAN and VDD_MAIN_PWR can be from external DC/DC converter or external LDO. However, I think, this also holds true for devices without internal LDO, e.g., LPC5526. They can also be powered from LDO or DC/DC converter. Don't you agree?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 07:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1728644#M54199</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-09-25T07:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: Using internal LDO instead of internal DCDC converter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1729264#M54208</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I agree with you that MCU can be powered from LDO or DC/DC even if there is not internal LDO or DC/Dc converter for MCU.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 02:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-Using-internal-LDO-instead-of-internal-DCDC-converter/m-p/1729264#M54208</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-26T02:15:01Z</dc:date>
    </item>
  </channel>
</rss>