<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cant Load Bootloader code on LPC11U67 MCU in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cant-Load-Bootloader-code-on-LPC11U67-MCU/m-p/1726775#M54158</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls try to use the following code and have a test.&lt;/P&gt;
&lt;P&gt;#define SYSCON_SYSAHBCLKCTRL (uint32_t *)0x40048080&lt;/P&gt;
&lt;P&gt;*SYSCON_SYSAHBCLKCTRL|=(1&amp;lt;&amp;lt;26) | (1 &amp;lt;&amp;lt; 27);&lt;/P&gt;
&lt;P&gt;I suppose that your SYSCON_SYSAHBCLKCTRL definition has issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 21 Sep 2023 06:06:03 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-09-21T06:06:03Z</dc:date>
    <item>
      <title>Cant Load Bootloader code on LPC11U67 MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cant-Load-Bootloader-code-on-LPC11U67-MCU/m-p/1725981#M54142</link>
      <description>&lt;P&gt;Hey,&lt;BR /&gt;&lt;BR /&gt;I'm using LPC11U67 MCU and trying to write a bootloader code.&lt;BR /&gt;I'm using function for deleting flash, wriing to flash and reading from flash.&amp;nbsp;&lt;BR /&gt;The build passed successfully, the issue is that the burn the program falls, and reach to the ResetISR function, where the line is:&lt;BR /&gt;*SYSCON_SYSAHBCLKCTRL |= (1&amp;lt;&amp;lt;26) | (1 &amp;lt;&amp;lt; 27);&lt;BR /&gt;&lt;BR /&gt;I&amp;nbsp; can't figure out what is the reason for this issue, can you please explain what should I check or do to solve this issue.&lt;BR /&gt;&lt;BR /&gt;Thanks in advance.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 06:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cant-Load-Bootloader-code-on-LPC11U67-MCU/m-p/1725981#M54142</guid>
      <dc:creator>Guy_mego</dc:creator>
      <dc:date>2023-09-20T06:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: Cant Load Bootloader code on LPC11U67 MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cant-Load-Bootloader-code-on-LPC11U67-MCU/m-p/1726775#M54158</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls try to use the following code and have a test.&lt;/P&gt;
&lt;P&gt;#define SYSCON_SYSAHBCLKCTRL (uint32_t *)0x40048080&lt;/P&gt;
&lt;P&gt;*SYSCON_SYSAHBCLKCTRL|=(1&amp;lt;&amp;lt;26) | (1 &amp;lt;&amp;lt; 27);&lt;/P&gt;
&lt;P&gt;I suppose that your SYSCON_SYSAHBCLKCTRL definition has issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 06:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cant-Load-Bootloader-code-on-LPC11U67-MCU/m-p/1726775#M54158</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-21T06:06:03Z</dc:date>
    </item>
  </channel>
</rss>