<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1788 and FLASHTIM value for 120MHz</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-and-FLASHTIM-value-for-120MHz/m-p/1725594#M54134</link>
    <description>&lt;P&gt;I want to run LPC1788 at 120MHz with IRC and PLL. From User Manual I read that I need to set PBOOST=3 and FLASHTIM=4 or 5. Of course, I can write:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;Chip_SYSCTL_EnableBoost();
Chip_SYSCTL_SetFLASHAccess(4 or 5);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Those functions are defined as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;STATIC INLINE void Chip_SYSCTL_EnableBoost(void)
{
	LPC_SYSCTL-&amp;gt;PBOOST = 0x3;
}

STATIC INLINE void Chip_SYSCTL_SetFLASHAccess(FMC_FLASHTIM_T clks)
{
	uint32_t tmp = LPC_SYSCTL-&amp;gt;FLASHCFG &amp;amp; 0xFFF;

	/* Don't alter lower bits */
	LPC_SYSCTL-&amp;gt;FLASHCFG = tmp | (clks &amp;lt;&amp;lt; 12);
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However LPCOpen defines FMC_FLASHTIM_T as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;typedef enum {
FLASHTIM_20MHZ_CPU = 0, /*!&amp;lt; Flash accesses use 1 CPU clocks. Use for up to 20 MHz CPU clock */
FLASHTIM_40MHZ_CPU = 1, /*!&amp;lt; Flash accesses use 2 CPU clocks. Use for up to 40 MHz CPU clock */
FLASHTIM_60MHZ_CPU = 2, /*!&amp;lt; Flash accesses use 3 CPU clocks. Use for up to 60 MHz CPU clock */
FLASHTIM_80MHZ_CPU = 3, /*!&amp;lt; Flash accesses use 4 CPU clocks. Use for up to 80 MHz CPU clock */
FLASHTIM_100MHZ_CPU = 4, /*!&amp;lt; Flash accesses use 5 CPU clocks. Use for up to 100 MHz CPU clock */
#if defined(CHIP_LPC177X_8X) || defined(CHIP_LPC40XX)
FLASHTIM_120MHZ_CPU = 3, /*!&amp;lt; Flash accesses use 4 CPU clocks. Use for up to 120 MHz CPU clock with power boot on*/
#else
FLASHTIM_120MHZ_CPU = 4, /*!&amp;lt; Flash accesses use 5 CPU clocks. Use for up to 120 Mhz for LPC1759 and LPC1769 only.*/
#endif
FLASHTIM_SAFE_SETTING = 5, /*!&amp;lt; Flash accesses use 6 CPU clocks. Safe setting for any allowed conditions */
} FMC_FLASHTIM_T;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems to me that definition of&amp;nbsp;FLASHTIM_120MHZ_CPU is faulty, because it is defined as 3 for CHIP_LPC177X_8X and CHIP_LPC40XX, instead of 4.&lt;/P&gt;&lt;P&gt;What is the right value to set FLASHTIM for 120MHz and power boost?&lt;/P&gt;</description>
    <pubDate>Tue, 19 Sep 2023 14:39:38 GMT</pubDate>
    <dc:creator>giusloq</dc:creator>
    <dc:date>2023-09-19T14:39:38Z</dc:date>
    <item>
      <title>LPC1788 and FLASHTIM value for 120MHz</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-and-FLASHTIM-value-for-120MHz/m-p/1725594#M54134</link>
      <description>&lt;P&gt;I want to run LPC1788 at 120MHz with IRC and PLL. From User Manual I read that I need to set PBOOST=3 and FLASHTIM=4 or 5. Of course, I can write:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;Chip_SYSCTL_EnableBoost();
Chip_SYSCTL_SetFLASHAccess(4 or 5);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Those functions are defined as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;STATIC INLINE void Chip_SYSCTL_EnableBoost(void)
{
	LPC_SYSCTL-&amp;gt;PBOOST = 0x3;
}

STATIC INLINE void Chip_SYSCTL_SetFLASHAccess(FMC_FLASHTIM_T clks)
{
	uint32_t tmp = LPC_SYSCTL-&amp;gt;FLASHCFG &amp;amp; 0xFFF;

	/* Don't alter lower bits */
	LPC_SYSCTL-&amp;gt;FLASHCFG = tmp | (clks &amp;lt;&amp;lt; 12);
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However LPCOpen defines FMC_FLASHTIM_T as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;typedef enum {
FLASHTIM_20MHZ_CPU = 0, /*!&amp;lt; Flash accesses use 1 CPU clocks. Use for up to 20 MHz CPU clock */
FLASHTIM_40MHZ_CPU = 1, /*!&amp;lt; Flash accesses use 2 CPU clocks. Use for up to 40 MHz CPU clock */
FLASHTIM_60MHZ_CPU = 2, /*!&amp;lt; Flash accesses use 3 CPU clocks. Use for up to 60 MHz CPU clock */
FLASHTIM_80MHZ_CPU = 3, /*!&amp;lt; Flash accesses use 4 CPU clocks. Use for up to 80 MHz CPU clock */
FLASHTIM_100MHZ_CPU = 4, /*!&amp;lt; Flash accesses use 5 CPU clocks. Use for up to 100 MHz CPU clock */
#if defined(CHIP_LPC177X_8X) || defined(CHIP_LPC40XX)
FLASHTIM_120MHZ_CPU = 3, /*!&amp;lt; Flash accesses use 4 CPU clocks. Use for up to 120 MHz CPU clock with power boot on*/
#else
FLASHTIM_120MHZ_CPU = 4, /*!&amp;lt; Flash accesses use 5 CPU clocks. Use for up to 120 Mhz for LPC1759 and LPC1769 only.*/
#endif
FLASHTIM_SAFE_SETTING = 5, /*!&amp;lt; Flash accesses use 6 CPU clocks. Safe setting for any allowed conditions */
} FMC_FLASHTIM_T;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems to me that definition of&amp;nbsp;FLASHTIM_120MHZ_CPU is faulty, because it is defined as 3 for CHIP_LPC177X_8X and CHIP_LPC40XX, instead of 4.&lt;/P&gt;&lt;P&gt;What is the right value to set FLASHTIM for 120MHz and power boost?&lt;/P&gt;</description>
      <pubDate>Tue, 19 Sep 2023 14:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-and-FLASHTIM-value-for-120MHz/m-p/1725594#M54134</guid>
      <dc:creator>giusloq</dc:creator>
      <dc:date>2023-09-19T14:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 and FLASHTIM value for 120MHz</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-and-FLASHTIM-value-for-120MHz/m-p/1725995#M54143</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160419"&gt;@giusloq&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please follow the UM. As the UM mentioned, FLASHTIM should be 0100 for operation from 100 to 120 MHz operation with power boost on.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 06:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-and-FLASHTIM-value-for-120MHz/m-p/1725995#M54143</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-09-20T06:59:33Z</dc:date>
    </item>
  </channel>
</rss>