<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC553x: ADC hardware trigger sources</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1725473#M54133</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206649"&gt;@RaRo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for getting back to me.&lt;/P&gt;&lt;P&gt;Let me please repeat in my own words what I learned from your notes:&lt;/P&gt;&lt;P&gt;Using "INPUTMUXER" registers, I route up to four trigger sources to each ADC (e.g., via registers&amp;nbsp;ADC0_TRIG0 - ADC0_TRIG3 for ADC0) selecting from 35 trigger inputs for each trigger source.&lt;/P&gt;&lt;P&gt;Then using "ADC" registers, for each trigger source that I routed above (up to four), I configure the ADC command that is triggered by that trigger source (e.g., via registers&amp;nbsp;TCTRL0 - TCTRL3).&lt;/P&gt;&lt;P&gt;That's different to the LPC552x with regard to routing trigger sources using the INPUTMUXER is not available on the LPC552x.&lt;/P&gt;&lt;P&gt;Did I understand this correctly?&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;PS: You seem to be looking at a different version of the manual than me.&amp;nbsp;This is what I'm looking at: Rev. 3, 07/2023&lt;/P&gt;&lt;P&gt;&lt;A href="https://cache.nxp.com/docs/en/reference-manual/LPC553xRM.pdf" target="_blank"&gt;https://cache.nxp.com/docs/en/reference-manual/LPC553xRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and there the ADC section has been moved to chapter 47:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielholala_0-1695109267205.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241572iAE583DFEE664575A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielholala_0-1695109267205.png" alt="danielholala_0-1695109267205.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielholala_0-1695109267205.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;PPS: If the reference manual could be a bit more elaborate instead of trying to be as concise as possible that would help and I would not need to raise these questions here. Nevertheless, I appreciate all the help I receive through the community forum. Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Sep 2023 11:10:34 GMT</pubDate>
    <dc:creator>danielholala</dc:creator>
    <dc:date>2023-09-19T11:10:34Z</dc:date>
    <item>
      <title>LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1723019#M54099</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;according to the manual, ADC hardware triggers can be generated from asynchronous input sources at the periphery of the ADC.&lt;/P&gt;&lt;P&gt;The reference manual reads: "The number and sources of hardware triggers implemented is device-specific. See the chip-specific ADC information for descriptions of available hardware trigger sources for this device."&lt;/P&gt;&lt;P&gt;I could not find the information the manual refers to.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where exactly is this "chip-specific ADC information" to be found?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Sep 2023 07:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1723019#M54099</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-09-15T07:42:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1724986#M54128</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/139806"&gt;@danielholala&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You could check the "&lt;EM&gt;chip-specific ADC information&lt;/EM&gt;" in the Datasheet and/or the User Manual of LPC553x. In this case, you could look the ADC Hardware Trigger information in the LPC553xRM.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;For the number and sources of hardware triggers available, please go to:&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;Section 46.2.2. Features,&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RaulRomero_0-1695073175200.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241490iEF905AD4781F6C08/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RaulRomero_0-1695073175200.png" alt="RaulRomero_0-1695073175200.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RaulRomero_0-1695073175200.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;[LPC553xRM. Chapter 46. Analog-to-Digital Converter (ADC)]&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;Section 46.1.4. ADC trigger inputs, and&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RaulRomero_1-1695073175201.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241491i22CD3A32005B8091/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RaulRomero_1-1695073175201.png" alt="RaulRomero_1-1695073175201.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RaulRomero_1-1695073175201.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;[LPC553xRM. Chapter 46. Analog-to-Digital Converter (ADC)]&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI class="lia-align-justify"&gt;Section 14.5.1.22 and 14.5.1.23. ADCx Trigger input connections.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 21:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1724986#M54128</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-09-18T21:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1725473#M54133</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206649"&gt;@RaRo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for getting back to me.&lt;/P&gt;&lt;P&gt;Let me please repeat in my own words what I learned from your notes:&lt;/P&gt;&lt;P&gt;Using "INPUTMUXER" registers, I route up to four trigger sources to each ADC (e.g., via registers&amp;nbsp;ADC0_TRIG0 - ADC0_TRIG3 for ADC0) selecting from 35 trigger inputs for each trigger source.&lt;/P&gt;&lt;P&gt;Then using "ADC" registers, for each trigger source that I routed above (up to four), I configure the ADC command that is triggered by that trigger source (e.g., via registers&amp;nbsp;TCTRL0 - TCTRL3).&lt;/P&gt;&lt;P&gt;That's different to the LPC552x with regard to routing trigger sources using the INPUTMUXER is not available on the LPC552x.&lt;/P&gt;&lt;P&gt;Did I understand this correctly?&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;PS: You seem to be looking at a different version of the manual than me.&amp;nbsp;This is what I'm looking at: Rev. 3, 07/2023&lt;/P&gt;&lt;P&gt;&lt;A href="https://cache.nxp.com/docs/en/reference-manual/LPC553xRM.pdf" target="_blank"&gt;https://cache.nxp.com/docs/en/reference-manual/LPC553xRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and there the ADC section has been moved to chapter 47:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielholala_0-1695109267205.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241572iAE583DFEE664575A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielholala_0-1695109267205.png" alt="danielholala_0-1695109267205.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielholala_0-1695109267205.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;PPS: If the reference manual could be a bit more elaborate instead of trying to be as concise as possible that would help and I would not need to raise these questions here. Nevertheless, I appreciate all the help I receive through the community forum. Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Sep 2023 11:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1725473#M54133</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-09-19T11:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1730452#M54229</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206649"&gt;@RaRo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;as ADC Trigger sources get routed through the &lt;EM&gt;Input Multiplexer&lt;/EM&gt;, I wonder where in &lt;STRONG&gt;Config Tools&lt;/STRONG&gt; do I configure these ADC Trigger sources?&lt;/P&gt;&lt;P&gt;Thanks.&lt;BR /&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 11:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1730452#M54229</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-09-27T11:09:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1732080#M54243</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/139806"&gt;@danielholala&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You are right, we were referring to a different RM of the one you point out. We apologize for the confusion. Please refer to &lt;EM&gt;Chapter 46. Analog-to-Digital Converter (ADC). Section 47.2.2. Features&lt;/EM&gt; and &lt;EM&gt;47.1.6. ADC trigger inputs&lt;/EM&gt;; and &lt;EM&gt;Chapter 14. Input Multiplexing (INPUTMUX). Section 14.5.1.1.20 ADC0 Trigger input connections&lt;/EM&gt;.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;&lt;EM&gt;Did I understand this correctly?&lt;/EM&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;Yes, according to the LPC553xRM that is the way to work with ADC trigger inputs.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Sep 2023 16:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1732080#M54243</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-09-29T16:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1732093#M54244</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/139806"&gt;@danielholala&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You could configure the ADC and the Trigger Source (e.g. CTimer) with ConfigTools Peripherals.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The INPUTMUX routing could be made through ConfigTools Pins, search for ADC0 -&amp;gt; TRIGx. Select the trigger source number you need and choose the trigger source which would create the INPUTMUX routing in the Code Preview.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RaulRomero_0-1696007114010.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/243266i7F9584F7E3D3812E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RaulRomero_0-1696007114010.png" alt="RaulRomero_0-1696007114010.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RaulRomero_0-1696007114010.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;[ConfigTools Pins -&amp;gt; INPUTMUX Trigger Sources]&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Sep 2023 17:06:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1732093#M54244</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-09-29T17:06:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x: ADC hardware trigger sources</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1733605#M54268</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206649"&gt;@RaRo&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;That's helpful. Thanks. I overlooked the "Peripheral Signals" tab of the Pins Tool.&lt;/P&gt;&lt;P&gt;Cheers&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 08:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-ADC-hardware-trigger-sources/m-p/1733605#M54268</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-10-04T08:04:09Z</dc:date>
    </item>
  </channel>
</rss>