<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックREG:Interface of J-Flash</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/REG-Interface-of-J-Flash/m-p/1723138#M54100</link>
    <description>&lt;P&gt;how can i connect jflash to program can any suggest.&lt;/P&gt;&lt;P&gt;Here we are using lpc54s018 microcontroller of 208pins and MCU Xpressoide .&lt;/P&gt;&lt;P&gt;In this jflash is used for programming.here target is connecting ,erase is also performing but is failed to program .can anyone worked on this controller reply me what could i made changes.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Sep 2023 12:31:16 GMT</pubDate>
    <dc:creator>faziya</dc:creator>
    <dc:date>2023-09-14T12:31:16Z</dc:date>
    <item>
      <title>REG:Interface of J-Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/REG-Interface-of-J-Flash/m-p/1723138#M54100</link>
      <description>&lt;P&gt;how can i connect jflash to program can any suggest.&lt;/P&gt;&lt;P&gt;Here we are using lpc54s018 microcontroller of 208pins and MCU Xpressoide .&lt;/P&gt;&lt;P&gt;In this jflash is used for programming.here target is connecting ,erase is also performing but is failed to program .can anyone worked on this controller reply me what could i made changes.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 12:31:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/REG-Interface-of-J-Flash/m-p/1723138#M54100</guid>
      <dc:creator>faziya</dc:creator>
      <dc:date>2023-09-14T12:31:16Z</dc:date>
    </item>
    <item>
      <title>Re: REG:Interface of J-Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/REG-Interface-of-J-Flash/m-p/1724637#M54120</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It appears that the J-Link can connect to qspi flash directly, but the the LPC54018JxM has internal flash, so the J-Link device can not connect to quad spi flash directly, so you can not use JFlash to program internal flash of LPC54018JxM directly.&lt;/P&gt;
&lt;P&gt;You can use blhost to program internal flash of LPC54018, pls refer to the doc&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 09:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/REG-Interface-of-J-Flash/m-p/1724637#M54120</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-18T09:34:28Z</dc:date>
    </item>
  </channel>
</rss>