<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S16- IO Expander in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-IO-Expander/m-p/1721672#M54075</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Am using lpc55s16, how to configure IO pin to IO expander, kindly guide to the configuration process&lt;/P&gt;</description>
    <pubDate>Wed, 13 Sep 2023 05:44:32 GMT</pubDate>
    <dc:creator>Sathiya_T</dc:creator>
    <dc:date>2023-09-13T05:44:32Z</dc:date>
    <item>
      <title>LPC55S16- IO Expander</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-IO-Expander/m-p/1721672#M54075</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Am using lpc55s16, how to configure IO pin to IO expander, kindly guide to the configuration process&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 05:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-IO-Expander/m-p/1721672#M54075</guid>
      <dc:creator>Sathiya_T</dc:creator>
      <dc:date>2023-09-13T05:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16- IO Expander</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-IO-Expander/m-p/1721745#M54079</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The LPC55S16 does not support I/O expander feature. For the LPC55S16, almost every signal is multiplexed with GPIO function, but the total GPIO pin number is totally dependent on package.&lt;/P&gt;
&lt;P&gt;If you want to expand I/O cell, you have to use the chip for example PCAL9554B or PCAL9554C which use I2C to expand I/O.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/data-sheet/PCAL9554B_PCAL9554C.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/data-sheet/PCAL9554B_PCAL9554C.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;it is okay to use a MCU with large package for example LPC54628, it has 208 pins, of course, a lot of GPIO pins.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc54000-arm-cortex-m4-:MC_1414576688124" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc54000-arm-cortex-m4-:MC_1414576688124&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;with each GPIO pin of LPC family, you can set or clear the pin logic in output mode, or input the pin logic in input mode.&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 06:51:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-IO-Expander/m-p/1721745#M54079</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-13T06:51:15Z</dc:date>
    </item>
  </channel>
</rss>