<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC54S018J4MET180 Ethernet doesn't work</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018J4MET180-Ethernet-doesn-t-work/m-p/1720972#M54065</link>
    <description>&lt;P&gt;Hi, &lt;SPAN&gt;I am currently debugging the Ethernet of the MCU&amp;nbsp;LPC54S018J4MET180 with RMII interface PHY, but it doesn't work ,and i found the ENET_RX_CLK (B5 pin)is floating, is it necessary to connect this pin with the PHY's REFCLOCK?&amp;nbsp; is there any way to make it work when&amp;nbsp;&amp;nbsp;ENET_RX_CLK is floating? thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Sep 2023 08:13:14 GMT</pubDate>
    <dc:creator>xiufengxing</dc:creator>
    <dc:date>2023-09-12T08:13:14Z</dc:date>
    <item>
      <title>LPC54S018J4MET180 Ethernet doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018J4MET180-Ethernet-doesn-t-work/m-p/1720972#M54065</link>
      <description>&lt;P&gt;Hi, &lt;SPAN&gt;I am currently debugging the Ethernet of the MCU&amp;nbsp;LPC54S018J4MET180 with RMII interface PHY, but it doesn't work ,and i found the ENET_RX_CLK (B5 pin)is floating, is it necessary to connect this pin with the PHY's REFCLOCK?&amp;nbsp; is there any way to make it work when&amp;nbsp;&amp;nbsp;ENET_RX_CLK is floating? thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 08:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018J4MET180-Ethernet-doesn-t-work/m-p/1720972#M54065</guid>
      <dc:creator>xiufengxing</dc:creator>
      <dc:date>2023-09-12T08:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54S018J4MET180 Ethernet doesn't work</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018J4MET180-Ethernet-doesn-t-work/m-p/1721577#M54074</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I copy the screenshot of the schematics of LPC54S018-EVK board, the crystal Y1 generates 25MHz clock with LAN8720A internal OSC circuit, with internal PLL, the LAN8720A outputs 50MHz clock to the pin 14 of&amp;nbsp; LAN8720A as REFCLKO clock signal, which is connected to PIO4_14 ENET_RX_CLK signal of LPC54018 with 180 pins package.&lt;/P&gt;
&lt;P&gt;In conclusion, the PIO4_14 ENET_RX_CLK signal of LPC54018 must be connected to a 50MHz clock from ethernet PHY so that they can synchronize.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1694574177685.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240690iD6F54E7EEB80F0F2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1694574177685.png" alt="xiangjun_rong_0-1694574177685.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1694574177685.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 03:11:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018J4MET180-Ethernet-doesn-t-work/m-p/1721577#M54074</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-13T03:11:11Z</dc:date>
    </item>
  </channel>
</rss>