<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Hard fault on LPC5526JBD64</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1717675#M54006</link>
    <description>&lt;P&gt;Hi Alice, I will have our embedded designer send you the project. Can you explain why we only see this on 1 of 4 boards? This issue is repeatable, but only on one board. The others do not have this issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 06 Sep 2023 04:36:13 GMT</pubDate>
    <dc:creator>jtauch1</dc:creator>
    <dc:date>2023-09-06T04:36:13Z</dc:date>
    <item>
      <title>Hard fault on LPC5526JBD64</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1710972#M53920</link>
      <description>&lt;P&gt;We have 4 boards that are being used for field testing. Of the 4, we have 1 board that deterministically encounters a hard fault. This occurs when the LPC attempts to access the UART peripheral. All 4 boards are running the same software build.&lt;/P&gt;&lt;P&gt;On the board in question when we write a char into an array index it induces a hard fault. The 3 other boards do not exhibit this behavior. The array size is 16384. When we start writing to indexes above 100 on the problematic board we begin seeing the fault.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could this indicate a hardware SRAM issue on this board?&lt;/P&gt;&lt;P&gt;I don't really see how a software issue could be so deterministic and only on one board.&lt;/P&gt;&lt;P&gt;We are continuing to debug this issue but wanted to see if anyone else had encountered this type of problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 20:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1710972#M53920</guid>
      <dc:creator>jtauch1</dc:creator>
      <dc:date>2023-08-24T20:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: Hard fault on LPC5526JBD64</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1711305#M53926</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/103551"&gt;@jtauch1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How about test simple SDK demo? Dose it can debug well?&lt;/P&gt;
&lt;P&gt;If SDK demo work well, only your own project hard fault, you can send your project to me, I help to check on my side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 25 Aug 2023 07:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1711305#M53926</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-08-25T07:53:50Z</dc:date>
    </item>
    <item>
      <title>Re: Hard fault on LPC5526JBD64</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1717675#M54006</link>
      <description>&lt;P&gt;Hi Alice, I will have our embedded designer send you the project. Can you explain why we only see this on 1 of 4 boards? This issue is repeatable, but only on one board. The others do not have this issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Sep 2023 04:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1717675#M54006</guid>
      <dc:creator>jtauch1</dc:creator>
      <dc:date>2023-09-06T04:36:13Z</dc:date>
    </item>
    <item>
      <title>Re: Hard fault on LPC5526JBD64</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1717846#M54011</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/103551"&gt;@jtauch1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If use same project, and the four boards are the same, how about check hardware connection for UART?&lt;/P&gt;
&lt;P&gt;If only one board has issue, I think there is no meaning about sending project to me, you should check hardware, also can first use a simple demo project test.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 06 Sep 2023 07:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1717846#M54011</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-09-06T07:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: Hard fault on LPC5526JBD64</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1719310#M54041</link>
      <description>&lt;P&gt;I've sent you our source i a private messge.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Sep 2023 07:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1719310#M54041</guid>
      <dc:creator>anbui</dc:creator>
      <dc:date>2023-09-08T07:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: Hard fault on LPC5526JBD64</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1720192#M54053</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/126448"&gt;@anbui&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have tested your project with LPCxpresso55s28-evk board, no hard fault, I think you need check hardware connection.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 08:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hard-fault-on-LPC5526JBD64/m-p/1720192#M54053</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-09-11T08:28:44Z</dc:date>
    </item>
  </channel>
</rss>