<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC845 under power during operation in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713715#M53961</link>
    <description>&lt;P&gt;&lt;EM&gt;&amp;gt; I note that we can use tools to simulate decreasing voltage or increasing internal resistance of the power supply. My colleagues are currently looking for these tools but can't find a "good" solution. Do you have a specific tool to suggest?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think several programmeable power supplies would easily allow for an endeavour.&lt;BR /&gt;But being a software guy, I don't have them either.&lt;BR /&gt;But I think a good lab power supply can do the job, turning the voltage and the current limit slowly down manually.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My point is, as the battery voltage decreases, the current capacity decreases simultaneously. The lower the voltage at MCU wake-up, the more drastic the effect on remaining capacity. Environment temperatures have an impact on battery behavior as well.&lt;BR /&gt;And Flash erase/write does significantly increase power consumption, making a fail and Flash corruption even more likely.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Though I don't know your application cycles and wake-up events. Perhaps you need to modify it to trigger the issue in a reasonable time in the lab.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 05:35:33 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2023-08-30T05:35:33Z</dc:date>
    <item>
      <title>LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1712480#M53939</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;As part of a project, I'm using the NXP LPC845 with the deep power down mode powered by a battery.&lt;/P&gt;&lt;P&gt;However, while doing some cycling tests, I encountered a problem.&lt;/P&gt;&lt;P&gt;The battery decreases and after a while the product doesn't work anymore. I decided to change the battery, but the product still didn't work.&lt;/P&gt;&lt;P&gt;Is it possible that if the microcontroller's power supply is too low, the flash will deteriorate, rendering the microcontroller unusable?&lt;/P&gt;&lt;P&gt;Has this ever happened to you?&lt;/P&gt;&lt;P&gt;Thank you in advance for the time you will devote to this topic and to the answers you will provide.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See u !&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 14:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1712480#M53939</guid>
      <dc:creator>MrVoxis</dc:creator>
      <dc:date>2023-08-28T14:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1712571#M53942</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197929"&gt;@MrVoxis&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using a development board or a custom board?&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;Is it possible that if the microcontroller's power supply is too low, the flash will deteriorate, rendering the microcontroller unusable?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No, low power supply should not be damaging neither the MCU nor the flash. Can you tell me the connections, the battery's voltaje and the project/example you are running? Does the LPC845 still detected by the PC when connected?&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 18:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1712571#M53942</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-08-28T18:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1712789#M53945</link>
      <description>&lt;P&gt;At some point, you will run into a brown-out, the MCU halts because the supply voltage is too low for proper operation.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt; I decided to change the battery, but the product still didn't work.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What is you application doing ?&lt;BR /&gt;Perhaps you are trying Flash erase/write operations, which increase the power consumption substantially. If a brown-out happens during such an operation, the Flash content might be corrupted.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would try to read out the Flash, and compare it with the original firmware you flashed it with.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 05:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1712789#M53945</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-08-29T05:39:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713050#M53948</link>
      <description>&lt;BR /&gt;Actually my application performs operations on the flash at very specific and dedicated addresses.&lt;BR /&gt;&lt;BR /&gt;The thing is that I protected the code in CRP2 so it's impossible to read the flash, I'll do this test with the project without this security and I'll let you know&lt;BR /&gt;&lt;BR /&gt;thank you for your reply</description>
      <pubDate>Tue, 29 Aug 2023 09:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713050#M53948</guid>
      <dc:creator>MrVoxis</dc:creator>
      <dc:date>2023-08-29T09:03:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713052#M53949</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Good morning, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks for reply, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I am using the nxp lpc845 for an embedded project. It is not recognized by the pc but this may be due to the CRP2 protection that I put. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I will do the test by removing this protection. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Otherwise the project is powered with a 3.3V flat battery&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 09:06:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713052#M53949</guid>
      <dc:creator>MrVoxis</dc:creator>
      <dc:date>2023-08-29T09:06:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713152#M53950</link>
      <description>&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;&amp;gt; I am using the nxp lpc845 for an embedded project. It is not recognized by the pc but this may be due to the CRP2 protection that I put.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Not sure if you mean on a PC (via USB), or with the toolchain.&lt;BR /&gt;The latter, i.e. LPCXpresso or another dev tool, would be my approach to read out the Flash.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Perhaps you can add some instrumentation code for testing, to see where the code fails during startup.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;&amp;gt; Otherwise the project is powered with a 3.3V flat battery.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;Since CRP is usually a hallmark of a commercial project, you supposedly have the tools to simulate the problem in a lab - i.e. slowly decreasing voltage and increasing internal resistance of the supply.&lt;BR /&gt;I think you could speed up the supply drop by orders of magnitude (seconds/minutes instead of weeks/months), and still observe the problem.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 10:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713152#M53950</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-08-29T10:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713355#M53953</link>
      <description>First of all, thank you for your answer.&lt;BR /&gt;&lt;BR /&gt;I've already implemented all these things but I'm using the "deep power down" mode and I've lost the debug and other things.&lt;BR /&gt;&lt;BR /&gt;I note that we can use tools to simulate decreasing voltage or increasing internal resistance of the power supply. My colleagues are currently looking for these tools but can't find a "good" solution. Do you have a specific tool to suggest?&lt;BR /&gt;&lt;BR /&gt;Have a nice day.&lt;BR /&gt;Bastien</description>
      <pubDate>Tue, 29 Aug 2023 15:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713355#M53953</guid>
      <dc:creator>MrVoxis</dc:creator>
      <dc:date>2023-08-29T15:09:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 under power during operation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713715#M53961</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; I note that we can use tools to simulate decreasing voltage or increasing internal resistance of the power supply. My colleagues are currently looking for these tools but can't find a "good" solution. Do you have a specific tool to suggest?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I think several programmeable power supplies would easily allow for an endeavour.&lt;BR /&gt;But being a software guy, I don't have them either.&lt;BR /&gt;But I think a good lab power supply can do the job, turning the voltage and the current limit slowly down manually.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My point is, as the battery voltage decreases, the current capacity decreases simultaneously. The lower the voltage at MCU wake-up, the more drastic the effect on remaining capacity. Environment temperatures have an impact on battery behavior as well.&lt;BR /&gt;And Flash erase/write does significantly increase power consumption, making a fail and Flash corruption even more likely.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Though I don't know your application cycles and wake-up events. Perhaps you need to modify it to trigger the issue in a reasonable time in the lab.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 05:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-under-power-during-operation/m-p/1713715#M53961</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-08-30T05:35:33Z</dc:date>
    </item>
  </channel>
</rss>