<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Project migration in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713407#M53956</link>
    <description>&lt;P&gt;Do you have both IDE versions still installed?&lt;BR /&gt;I was caught out by this that although the workspace and projects were independent the SDKs were installed in a "default common area" - what happened in my case is that the 2.14 SDK will&amp;nbsp;&lt;EM&gt;only&lt;/EM&gt; be accepted by the 11.8 IDE, but it is in the common space...&lt;/P&gt;&lt;P&gt;If you open the older IDE it will attempt to load the SDK, report that it can't, and then the default behaviour is to delete the offending SDK.&lt;/P&gt;&lt;P&gt;I found it caused a lot of problems having both IDE installed at the same time (or at least opening the older IDE once I'd installed the new SDKs caused problems).&lt;/P&gt;</description>
    <pubDate>Tue, 29 Aug 2023 17:44:04 GMT</pubDate>
    <dc:creator>PhilV</dc:creator>
    <dc:date>2023-08-29T17:44:04Z</dc:date>
    <item>
      <title>Project migration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713335#M53952</link>
      <description>&lt;P&gt;Currently using MCUXpresso 11.5 with SDK 2.11.&amp;nbsp; I would like to migrate to 11.8 / 2.14.&amp;nbsp; Is there a whitepaper or something on how to best migrate my existing BSP and applicaiton code?&amp;nbsp; I really don't want to lose that and have to start all over from scratch.&amp;nbsp; Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 14:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713335#M53952</guid>
      <dc:creator>JK_265</dc:creator>
      <dc:date>2023-08-29T14:34:52Z</dc:date>
    </item>
    <item>
      <title>Re: Project migration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713380#M53954</link>
      <description>&lt;P&gt;I decided to move ahead with installing the 11.8 version of MCUXpresso and a new SDK.&amp;nbsp; Based on what I have seen previously, there was pretty good isolation between old and new versions.&amp;nbsp; I installed MCUXpresso 11.8, but when I try to import a pre-downloaded SDK for LPC5514 (SDK version 2.14), it copies the ZIP file but that's it - it does not list the micro under the proper tab for a new project.&amp;nbsp; If I try to create a new project and have it pull the SDK directly from NXP I got the following error at the end of the install:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JK_265_0-1693326568688.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238723i38EBBB35451366B2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JK_265_0-1693326568688.png" alt="JK_265_0-1693326568688.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JK_265_0-1693326568688.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any ideas what is going on?&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 16:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713380#M53954</guid>
      <dc:creator>JK_265</dc:creator>
      <dc:date>2023-08-29T16:30:49Z</dc:date>
    </item>
    <item>
      <title>Re: Project migration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713407#M53956</link>
      <description>&lt;P&gt;Do you have both IDE versions still installed?&lt;BR /&gt;I was caught out by this that although the workspace and projects were independent the SDKs were installed in a "default common area" - what happened in my case is that the 2.14 SDK will&amp;nbsp;&lt;EM&gt;only&lt;/EM&gt; be accepted by the 11.8 IDE, but it is in the common space...&lt;/P&gt;&lt;P&gt;If you open the older IDE it will attempt to load the SDK, report that it can't, and then the default behaviour is to delete the offending SDK.&lt;/P&gt;&lt;P&gt;I found it caused a lot of problems having both IDE installed at the same time (or at least opening the older IDE once I'd installed the new SDKs caused problems).&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 17:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713407#M53956</guid>
      <dc:creator>PhilV</dc:creator>
      <dc:date>2023-08-29T17:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: Project migration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713445#M53957</link>
      <description>&lt;P&gt;So, I think that got through what I would call the 'cohabitation' problem:&lt;/P&gt;&lt;P&gt;0) Leave the old version of MCUXpresso alone.&amp;nbsp; Probably best to close it.&lt;BR /&gt;1) Download the 2.14 SDK, making sure to select the option for MCUXpresso during generation.&lt;BR /&gt;2) Make a folder of your choice like ...\mcuxpresso\SDK_2.14\SDKPackages&lt;BR /&gt;3) Copy the SDK ZIP file to that folder and expand all the contents there&lt;BR /&gt;4) Open MCUXpresso, and go to Windows-&amp;gt;Preferences and burrow down to the following setting.&amp;nbsp; Add the folder in step #2, and bump it to the front of the list.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JK_265_0-1693335200668.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238734i3655107E051B4878/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JK_265_0-1693335200668.png" alt="JK_265_0-1693335200668.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JK_265_0-1693335200668.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;5) Restart the new version of the MCUXpresso.&lt;/P&gt;&lt;P&gt;Having said that, I could still use some guidance on how to best import the existing MCUXpresso project into version 11.8.&amp;nbsp; I have modified the project heavily to feed the output into IAR.&amp;nbsp; I don't build within MCUXpresso - just use the configuration tools and code generation capabilities to feed into the IAR workflow.&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 18:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Project-migration/m-p/1713445#M53957</guid>
      <dc:creator>JK_265</dc:creator>
      <dc:date>2023-08-29T18:53:32Z</dc:date>
    </item>
  </channel>
</rss>