<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC844 ISP entry pin timing</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-ISP-entry-pin-timing/m-p/1707525#M53881</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've a rather large capacitor connected to the ISP entry pin due to EMC issues. I'm using an LPC844.&lt;/P&gt;&lt;P&gt;I now have the problem that the part sometimes enters ISP mode on boot due to the capacitor not charging fast enough.&lt;/P&gt;&lt;P&gt;Is there any timing information available for the ISP entry pin so I can make sure that either the capacitor gets charged fast enough or that the reset signal is delay just long enough?&lt;/P&gt;&lt;P&gt;Please note that I want to keep the ISP entry feature, as there is also a button connected to force ISP mode. So I can't just disable it in FAIM/CRP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Remco Poelstra&lt;/P&gt;</description>
    <pubDate>Fri, 18 Aug 2023 11:55:30 GMT</pubDate>
    <dc:creator>r_poelstra</dc:creator>
    <dc:date>2023-08-18T11:55:30Z</dc:date>
    <item>
      <title>LPC844 ISP entry pin timing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-ISP-entry-pin-timing/m-p/1707525#M53881</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've a rather large capacitor connected to the ISP entry pin due to EMC issues. I'm using an LPC844.&lt;/P&gt;&lt;P&gt;I now have the problem that the part sometimes enters ISP mode on boot due to the capacitor not charging fast enough.&lt;/P&gt;&lt;P&gt;Is there any timing information available for the ISP entry pin so I can make sure that either the capacitor gets charged fast enough or that the reset signal is delay just long enough?&lt;/P&gt;&lt;P&gt;Please note that I want to keep the ISP entry feature, as there is also a button connected to force ISP mode. So I can't just disable it in FAIM/CRP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Remco Poelstra&lt;/P&gt;</description>
      <pubDate>Fri, 18 Aug 2023 11:55:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-ISP-entry-pin-timing/m-p/1707525#M53881</guid>
      <dc:creator>r_poelstra</dc:creator>
      <dc:date>2023-08-18T11:55:30Z</dc:date>
    </item>
  </channel>
</rss>