<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC51U68 ADC maximum performance in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705601#M53861</link>
    <description>&lt;BR /&gt;&lt;BR /&gt;Example checked.&lt;BR /&gt;The example seems to be 100*50000 for 5MSPS.&lt;BR /&gt;It works fine.&lt;BR /&gt;The problem will not be debugged if you set it to 10 or 1 in SAMPLENUM 100.&lt;BR /&gt;Increasing SAMPLENUM causes memory problems&lt;BR /&gt;I'll take that into consideration. Thank you.</description>
    <pubDate>Wed, 16 Aug 2023 08:48:08 GMT</pubDate>
    <dc:creator>bonsani</dc:creator>
    <dc:date>2023-08-16T08:48:08Z</dc:date>
    <item>
      <title>LPC51U68 ADC maximum performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705384#M53855</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Referring to the LPC51U68 datasheet, it is said to have ADC 5MSPS, but it actually comes out to about 200KSPS. Based on 2 channels&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there an example code to refer to?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 05:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705384#M53855</guid>
      <dc:creator>bonsani</dc:creator>
      <dc:date>2023-08-16T05:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 ADC maximum performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705512#M53857</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As the following screenshot, the ADC clock can reach up to 80mhz, one ADC conversion needs 15 clock cycles, so the ADC sampling rate can be 80Mhz/15=5MSPS.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1692171220074.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236637iA0BE048FE29F6107/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1692171220074.png" alt="xiangjun_rong_0-1692171220074.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you want to get maximum 5MSPS, you can not use the interrupt mode, because the LPC51U68 interrupt rate can not reach up to 5mhz.&lt;/P&gt;
&lt;P&gt;You can use DMA to transfer the ADC result if the ADC conversion rate is up to 5MHz.&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 07:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705512#M53857</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-08-16T07:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 ADC maximum performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705560#M53858</link>
      <description>The ADC DMA example included in SDK 2.8.2 does not work until 5MSPS. DMA interrupt occurs.</description>
      <pubDate>Wed, 16 Aug 2023 08:15:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705560#M53858</guid>
      <dc:creator>bonsani</dc:creator>
      <dc:date>2023-08-16T08:15:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 ADC maximum performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705575#M53860</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I just modified the lpc_adc_dma with burst mode so that you can sample ADC&amp;nbsp; channel multiple times.&lt;/P&gt;
&lt;P&gt;It appears working.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 08:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705575#M53860</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-08-16T08:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 ADC maximum performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705601#M53861</link>
      <description>&lt;BR /&gt;&lt;BR /&gt;Example checked.&lt;BR /&gt;The example seems to be 100*50000 for 5MSPS.&lt;BR /&gt;It works fine.&lt;BR /&gt;The problem will not be debugged if you set it to 10 or 1 in SAMPLENUM 100.&lt;BR /&gt;Increasing SAMPLENUM causes memory problems&lt;BR /&gt;I'll take that into consideration. Thank you.</description>
      <pubDate>Wed, 16 Aug 2023 08:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1705601#M53861</guid>
      <dc:creator>bonsani</dc:creator>
      <dc:date>2023-08-16T08:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 ADC maximum performance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1707109#M53876</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The answer is yes, in burst mode, the ADC will continue to sample one by one, so in burst mode, you can not control the ADC conversion rate.&lt;/P&gt;
&lt;P&gt;In Fig 79 ADC block diagram, the SCT0 output 7 can trigger ADC, if you want to control the ADC sampling frequency, you have to disable the burst mode, use the hardware triggering mode, the hardware triggering source is SCT0 output 7, so the SCT0 can define the ADC conversion rate. But you have to develop code for the SCT0 output 7 so that it can output PWM signal to trigger ADC.&lt;/P&gt;
&lt;P&gt;The SDK has both SCT and ADC code&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 18 Aug 2023 01:35:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-ADC-maximum-performance/m-p/1707109#M53876</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-08-18T01:35:10Z</dc:date>
    </item>
  </channel>
</rss>