<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC2460 XTAL2 output in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2460-XTAL2-output/m-p/1705354#M53854</link>
    <description>&lt;P&gt;We are using the LPC2460 in Slave mode operation with a 12mhz crystal clock oscillator driving the XTAL1 input. In this mode, what is the output of the XTAL2 pin ?&lt;/P&gt;</description>
    <pubDate>Wed, 16 Aug 2023 03:49:38 GMT</pubDate>
    <dc:creator>kevinbooh</dc:creator>
    <dc:date>2023-08-16T03:49:38Z</dc:date>
    <item>
      <title>LPC2460 XTAL2 output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2460-XTAL2-output/m-p/1705354#M53854</link>
      <description>&lt;P&gt;We are using the LPC2460 in Slave mode operation with a 12mhz crystal clock oscillator driving the XTAL1 input. In this mode, what is the output of the XTAL2 pin ?&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 03:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2460-XTAL2-output/m-p/1705354#M53854</guid>
      <dc:creator>kevinbooh</dc:creator>
      <dc:date>2023-08-16T03:49:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2460 XTAL2 output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2460-XTAL2-output/m-p/1705418#M53856</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For LPC2460, in slave mode, you connect a clock source to the XTAL1 pin via a capacitor Ci with XTAL2 pin float as the following fig:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1692165954087.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236610i4CEF846FC1C1A270/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1692165954087.png" alt="xiangjun_rong_0-1692165954087.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1692165954087.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In the case, the XTAL2 pin will output a sine signal with the same clock source frequency, but there is a phase-shift.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 06:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2460-XTAL2-output/m-p/1705418#M53856</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-08-16T06:08:28Z</dc:date>
    </item>
  </channel>
</rss>