<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックDisabling multicore on an LPC55S69 project</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disabling-multicore-on-an-LPC55S69-project/m-p/1698838#M53706</link>
    <description>&lt;P&gt;Hello -&lt;/P&gt;&lt;P&gt;I have a project that I'm working on under MCUXpresso v11.6.1. The project was initially created as a multicore project. I want to undo that and have the project configured just to run on core0. How can I do that? The documentation seems to be silent on this.&lt;/P&gt;&lt;P&gt;Is it possible to re-run the project configuration wizard to update the configuration of an existing project?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;John Sambrook&lt;/P&gt;</description>
    <pubDate>Thu, 03 Aug 2023 18:25:16 GMT</pubDate>
    <dc:creator>jsambrook</dc:creator>
    <dc:date>2023-08-03T18:25:16Z</dc:date>
    <item>
      <title>Disabling multicore on an LPC55S69 project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disabling-multicore-on-an-LPC55S69-project/m-p/1698838#M53706</link>
      <description>&lt;P&gt;Hello -&lt;/P&gt;&lt;P&gt;I have a project that I'm working on under MCUXpresso v11.6.1. The project was initially created as a multicore project. I want to undo that and have the project configured just to run on core0. How can I do that? The documentation seems to be silent on this.&lt;/P&gt;&lt;P&gt;Is it possible to re-run the project configuration wizard to update the configuration of an existing project?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;John Sambrook&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 18:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Disabling-multicore-on-an-LPC55S69-project/m-p/1698838#M53706</guid>
      <dc:creator>jsambrook</dc:creator>
      <dc:date>2023-08-03T18:25:16Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling multicore on an LPC55S69 project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disabling-multicore-on-an-LPC55S69-project/m-p/1699974#M53743</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding your requirement to remove the code for the core1 and just keep the code of core0, I think there are two methods, you can create a new project with just core0 and copy the code in the old project for just core0 and remove the code like MCMGR......... and the erpc.....&lt;/P&gt;
&lt;P&gt;The second method is to unload the project for the core1 in MCUXPresso tools. For the project for core0, just&amp;nbsp; delete the the code like MCMGR......... and the erpc....., in the MultiCore menu, uncheck the slave box.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1691392563408.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235291i709EF5E01B0F89FA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1691392563408.png" alt="xiangjun_rong_0-1691392563408.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it is helpful&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 07:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Disabling-multicore-on-an-LPC55S69-project/m-p/1699974#M53743</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-08-07T07:18:48Z</dc:date>
    </item>
  </channel>
</rss>