<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: USB Mass Storage Class Device Example on LPCOpen 2.05</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1698386#M53694</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thanks for the reply. Could you please share UM document? Also, I found below link which has MSC example for LPC11xx, so can I use this example as reference for development I hope same API's are available for LPC1347.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPCopen-2-x-and-USB-Mass-Storage/m-p/523836?profile.language=en" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPCopen-2-x-and-USB-Mass-Storage/m-p/523836?profile.language=en&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vijay Rakesh.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Aug 2023 07:42:48 GMT</pubDate>
    <dc:creator>vrakeshm13</dc:creator>
    <dc:date>2023-08-03T07:42:48Z</dc:date>
    <item>
      <title>USB Mass Storage Class Device Example on LPCOpen 2.05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1697230#M53680</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any USB Mass Storage Class Device example available for LPC1347 on LPCOpen v2.05? Kindly please share if it is available.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Rakesh&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 06:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1697230#M53680</guid>
      <dc:creator>vrakeshm13</dc:creator>
      <dc:date>2023-08-02T06:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage Class Device Example on LPCOpen 2.05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1698377#M53693</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220055"&gt;@vrakeshm13&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry there is no MSC example for lpc1437, there is usbd MSC API in UM-&amp;gt; 11.5.35&amp;nbsp;USBD_MSC_API and 11.5.36.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 07:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1698377#M53693</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-08-03T07:25:49Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage Class Device Example on LPCOpen 2.05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1698386#M53694</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thanks for the reply. Could you please share UM document? Also, I found below link which has MSC example for LPC11xx, so can I use this example as reference for development I hope same API's are available for LPC1347.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPCopen-2-x-and-USB-Mass-Storage/m-p/523836?profile.language=en" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPCopen-2-x-and-USB-Mass-Storage/m-p/523836?profile.language=en&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vijay Rakesh.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 07:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1698386#M53694</guid>
      <dc:creator>vrakeshm13</dc:creator>
      <dc:date>2023-08-03T07:42:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage Class Device Example on LPCOpen 2.05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1700090#M53749</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220055"&gt;@vrakeshm13&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you can refer to it.The APIs almost the same, they are USB ROM API.&lt;/P&gt;
&lt;P&gt;UM meaning UM10524. The APIs are included in LPCopen.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 09:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Class-Device-Example-on-LPCOpen-2-05/m-p/1700090#M53749</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-08-07T09:24:14Z</dc:date>
    </item>
  </channel>
</rss>