<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB audio distortion on LPC5411X in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1693700#M53605</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you do not change anything, do the sound distortion happen or not?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jul 2023 02:31:45 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-07-27T02:31:45Z</dc:date>
    <item>
      <title>USB audio distortion on LPC5411X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1689046#M53501</link>
      <description>&lt;P&gt;We have a periodic audio distortion with USB Audio device on LPC54114 MCU (OM13090). The issue can be seen in recorded stream and can be listened on speaker. The period is 4-38 min. The distortion time is 2-5 secs. Codec is WM8904. Sample rate is 16kHz.&lt;/P&gt;&lt;P&gt;The board was connected to PC with Ubuntu 20.04. The example project is lpcxpresso54114_rom_dev_audio_bm.&lt;/P&gt;&lt;P&gt;There are only two changes: 1) Uncommented sine in function void i2s_read(void) in i2s_if.c; 2) Changed divider of sine from 28 to 1 in sine_file.c.&lt;/P&gt;&lt;P&gt;Recording of test audio file was made by command: =&amp;gt; arecord -f dat -r 16000 test_ref_1.wav.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 06:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1689046#M53501</guid>
      <dc:creator>Kirill_klk</dc:creator>
      <dc:date>2023-07-20T06:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: USB audio distortion on LPC5411X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1693700#M53605</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you do not change anything, do the sound distortion happen or not?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jul 2023 02:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1693700#M53605</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-07-27T02:31:45Z</dc:date>
    </item>
    <item>
      <title>回复： USB audio distortion on LPC5411X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1695702#M53650</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It is very difficult to reproduce the issue on Windows. We found it only 2 times with and without changes in code. On Linux the situation is worse. We found the issue each time when start recording.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jul 2023 08:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-audio-distortion-on-LPC5411X/m-p/1695702#M53650</guid>
      <dc:creator>Kirill_klk</dc:creator>
      <dc:date>2023-07-31T08:41:31Z</dc:date>
    </item>
  </channel>
</rss>