<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHow to write 1 byte of data into external flash in LPC4370 board</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-write-1-byte-of-data-into-external-flash-in-LPC4370-board/m-p/1692920#M53593</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to write a constant value like a "Device ID" into the flash memory which would never be changed or modified even when the board is Reset/ ON. Please help me how to do it&lt;BR /&gt;I was thinking to use SPIFI for this, but i still didnt understand how we can store the Device ID data into a particular address of the Flash memory and can be accesses/read later.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Please note: that LPC4370 have external flash only no internal flash&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 09:10:42 GMT</pubDate>
    <dc:creator>mathewcigi</dc:creator>
    <dc:date>2023-07-26T09:10:42Z</dc:date>
    <item>
      <title>How to write 1 byte of data into external flash in LPC4370 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-write-1-byte-of-data-into-external-flash-in-LPC4370-board/m-p/1692920#M53593</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to write a constant value like a "Device ID" into the flash memory which would never be changed or modified even when the board is Reset/ ON. Please help me how to do it&lt;BR /&gt;I was thinking to use SPIFI for this, but i still didnt understand how we can store the Device ID data into a particular address of the Flash memory and can be accesses/read later.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Please note: that LPC4370 have external flash only no internal flash&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 09:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-write-1-byte-of-data-into-external-flash-in-LPC4370-board/m-p/1692920#M53593</guid>
      <dc:creator>mathewcigi</dc:creator>
      <dc:date>2023-07-26T09:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to write 1 byte of data into external flash in LPC4370 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-write-1-byte-of-data-into-external-flash-in-LPC4370-board/m-p/1695803#M53651</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199731"&gt;@mathewcigi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you referring this thread&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/RODATA-array-data-missing-filled-with-zeros/m-p/832821" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/RODATA-array-data-missing-filled-with-zeros/m-p/832821&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jul 2023 09:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-write-1-byte-of-data-into-external-flash-in-LPC4370-board/m-p/1695803#M53651</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-07-31T09:51:38Z</dc:date>
    </item>
  </channel>
</rss>