<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What could be practical reason for using two 1MB Static RAM chips on LPC1788? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1691402#M53552</link>
    <description>&lt;P&gt;Thank you, Alice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These chips are used for background and foreground frames for LCD so, if one were broken the entire board would stop functioning…&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;</description>
    <pubDate>Mon, 24 Jul 2023 12:50:51 GMT</pubDate>
    <dc:creator>Eugene723</dc:creator>
    <dc:date>2023-07-24T12:50:51Z</dc:date>
    <item>
      <title>What could be practical reason for using two 1MB Static RAM chips on LPC1788?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1690445#M53518</link>
      <description>&lt;P&gt;I recently took on support for a board designed by others about 10 years ago. There are two 8Mbit (1MB) CY7C1051 chips on this board.&lt;/P&gt;&lt;P&gt;LPC1788 has four Chip Selects (CS0 through CS3) each supporting up to 64MB of static RAM.&lt;/P&gt;&lt;P&gt;I don’t have much hardware design knowledge hence my question. I briefly checked on pricing and noticed that one 4MB chip costs about as much as two 1MB while providing two times memory amount.&lt;/P&gt;&lt;P&gt;What could be the reason to design two separate 1MB chips as opposite to one of a larger size?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jul 2023 12:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1690445#M53518</guid>
      <dc:creator>Eugene723</dc:creator>
      <dc:date>2023-07-21T12:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: What could be practical reason for using two 1MB Static RAM chips on LPC1788?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1691391#M53551</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206134"&gt;@Eugene723&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Maybe one SRAM is broken, anther one can used.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also for the chip costs, you need check the same company and same series.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jul 2023 12:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1691391#M53551</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-07-24T12:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: What could be practical reason for using two 1MB Static RAM chips on LPC1788?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1691402#M53552</link>
      <description>&lt;P&gt;Thank you, Alice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These chips are used for background and foreground frames for LCD so, if one were broken the entire board would stop functioning…&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jul 2023 12:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1691402#M53552</guid>
      <dc:creator>Eugene723</dc:creator>
      <dc:date>2023-07-24T12:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: What could be practical reason for using two 1MB Static RAM chips on LPC1788?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1692121#M53575</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206134"&gt;@Eugene723&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; For LPC1788, no such limitation.&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;one 4MB chip costs about as much as two 1MB while providing two times memory amount.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; Recommend using one 4MB chip as this situation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 08:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-could-be-practical-reason-for-using-two-1MB-Static-RAM/m-p/1692121#M53575</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-07-25T08:57:35Z</dc:date>
    </item>
  </channel>
</rss>