<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCan't able to generate clock</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1686617#M53456</link>
    <description>&lt;P&gt;Hi Everyone!&lt;/P&gt;&lt;P&gt;I am using LPC54S0JBD208 controller in my project as intial stage i have installed ExpressoIDE and later SDC&lt;/P&gt;&lt;P&gt;and after that i tried to select the development board of LPC54SO18 development board as there is no option to select the directcontroller later in project configuration i selected&amp;nbsp;&amp;nbsp;LPC54S0JBD208 controller during this time IDe throw a warning ie.,&amp;nbsp;Board configuration files (such as pin-mux and clock-config) are not designed and might not work with the selected device. It's recommended to use Empty Board Files instead.&lt;/P&gt;&lt;P&gt;I selected emptyboardfiles this time it given another warning ie.,&amp;nbsp; Choosing empty board files may cause the absence of some defines (eg. BOARD_FLASH_SIZE). so i neglected that warning and created project later i opened clock configuration in IDE and tried to configure clock but it is always thowing an error&amp;nbsp;&lt;/P&gt;&lt;P&gt;are there any videos /document to generate clock for this controller if so please share for refering.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;ANIL&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 11:55:38 GMT</pubDate>
    <dc:creator>faziya</dc:creator>
    <dc:date>2023-07-12T11:55:38Z</dc:date>
    <item>
      <title>Can't able to generate clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1686617#M53456</link>
      <description>&lt;P&gt;Hi Everyone!&lt;/P&gt;&lt;P&gt;I am using LPC54S0JBD208 controller in my project as intial stage i have installed ExpressoIDE and later SDC&lt;/P&gt;&lt;P&gt;and after that i tried to select the development board of LPC54SO18 development board as there is no option to select the directcontroller later in project configuration i selected&amp;nbsp;&amp;nbsp;LPC54S0JBD208 controller during this time IDe throw a warning ie.,&amp;nbsp;Board configuration files (such as pin-mux and clock-config) are not designed and might not work with the selected device. It's recommended to use Empty Board Files instead.&lt;/P&gt;&lt;P&gt;I selected emptyboardfiles this time it given another warning ie.,&amp;nbsp; Choosing empty board files may cause the absence of some defines (eg. BOARD_FLASH_SIZE). so i neglected that warning and created project later i opened clock configuration in IDE and tried to configure clock but it is always thowing an error&amp;nbsp;&lt;/P&gt;&lt;P&gt;are there any videos /document to generate clock for this controller if so please share for refering.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;ANIL&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 11:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1686617#M53456</guid>
      <dc:creator>faziya</dc:creator>
      <dc:date>2023-07-12T11:55:38Z</dc:date>
    </item>
    <item>
      <title>Re: Can't able to generate clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1716274#M53987</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215308"&gt;@faziya&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry to reply late, because there is issue with our network for that days, so missed your case, sorry.&lt;/P&gt;
&lt;P&gt;If still have issue, please tell me, I will help you, thanks.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 07:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1716274#M53987</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-09-04T07:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: Can't able to generate clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1819603#M55537</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;,I have similar problem could you please help me ?&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 14:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-able-to-generate-clock/m-p/1819603#M55537</guid>
      <dc:creator>koray692</dc:creator>
      <dc:date>2024-03-01T14:42:35Z</dc:date>
    </item>
  </channel>
</rss>