<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC54113 Controller RAM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686264#M53444</link>
    <description>&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the LPC54113 Controller RAM Area is erased by the software, Watchdog Reset time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;B Pavan Kumar&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 06:07:44 GMT</pubDate>
    <dc:creator>PK_1114</dc:creator>
    <dc:date>2023-07-12T06:07:44Z</dc:date>
    <item>
      <title>LPC54113 Controller RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686264#M53444</link>
      <description>&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the LPC54113 Controller RAM Area is erased by the software, Watchdog Reset time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;B Pavan Kumar&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 06:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686264#M53444</guid>
      <dc:creator>PK_1114</dc:creator>
      <dc:date>2023-07-12T06:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54113 Controller RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686371#M53446</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that there is not erasing concept for SRAM,you can write any data at any time to an address of SRAM. In&amp;nbsp; general, after reset, the data in SRAM is random, even if the data in SRAM are all zero, you can not take it for granted.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 07:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686371#M53446</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-07-12T07:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54113 Controller RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686406#M53448</link>
      <description>&lt;P&gt;To expand on that, SRAM is usually initialized in the startup code.&lt;BR /&gt;Most regions are cleared (to zero), others are initialized with constant data from Flash, according to the linker script settings.&lt;/P&gt;&lt;P&gt;If one want to change this behavior, this would be the place to implement it, i.e. the startup code in connection with the linker script and section definitions.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 08:25:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-Controller-RAM/m-p/1686406#M53448</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-07-12T08:25:23Z</dc:date>
    </item>
  </channel>
</rss>