<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using 1 LPC4322 to debug both LPC55S69 and QN9090 on a Custom PCB Board in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1686186#M53443</link>
    <description>&lt;P&gt;Thank you for the clarification.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 03:45:47 GMT</pubDate>
    <dc:creator>SrinathVelavan</dc:creator>
    <dc:date>2023-07-12T03:45:47Z</dc:date>
    <item>
      <title>Using 1 LPC4322 to debug both LPC55S69 and QN9090 on a Custom PCB Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1685879#M53435</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am developing a custom PCB board with LPC55S69 as the host MCU. Inorder to debug my SDK, I am using LPC4322 as used by the EVK board of LPC55S69. Now, I am including QN9090 as part of my custom board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the DK006 QN9090 development kit, LPC4322 is used as a debugger for linking to QN9090 chip.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I use 1 LPC4322 to debug both my LPC55S69 and QN9090 using the SWD interface? If so, should I use the same SWD pins or can I configure the GPIO pins of LPC4322 to pinout 2 separate SWD pins (1 for LPC55S69 and 1 for QN9090)? Is this possible to do or should I use 2 separate LPC4322 debugger chips on my custom board??&lt;/P&gt;&lt;P&gt;Please help with this query.&lt;/P&gt;&lt;P&gt;TIA&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 15:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1685879#M53435</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-07-11T15:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: Using 1 LPC4322 to debug both LPC55S69 and QN9090 on a Custom PCB Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1685931#M53436</link>
      <description>&lt;P&gt;Unlike JTAG, SWD is not designed to debug multiple devices in a daisy chain or other ways. I suggest you add two SWD ports with two debug probes attached.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 17:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1685931#M53436</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-07-11T17:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: Using 1 LPC4322 to debug both LPC55S69 and QN9090 on a Custom PCB Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1686186#M53443</link>
      <description>&lt;P&gt;Thank you for the clarification.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 03:45:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-1-LPC4322-to-debug-both-LPC55S69-and-QN9090-on-a-Custom/m-p/1686186#M53443</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-07-12T03:45:47Z</dc:date>
    </item>
  </channel>
</rss>