<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S6x USB1 as full speed device in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-USB1-as-full-speed-device/m-p/1680697#M53311</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I see in this topic...&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537&lt;/A&gt;&lt;/P&gt;&lt;P&gt;that USB1 can't be forced to device in full speed mode, but there is in user manual (UM11126),&amp;nbsp;Table 834. USB1 device command/status register (DEVCMDSTAT) bit 21 (R/W):&lt;/P&gt;&lt;P&gt;Forced FS&lt;/P&gt;&lt;P&gt;0: Default - drive K chirp during reset, go through HS negotiation.&lt;/P&gt;&lt;P&gt;1: Force the device to FS, do not drive K chirp during reset.&lt;/P&gt;&lt;P&gt;If USB1 device can be forced to full speed, in this case USB1 controller supporting crystal-less operation like USB0 or not? With both USB0 and USB1 active as full speed device.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JH&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jul 2023 19:50:04 GMT</pubDate>
    <dc:creator>jh0</dc:creator>
    <dc:date>2023-07-03T19:50:04Z</dc:date>
    <item>
      <title>LPC55S6x USB1 as full speed device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-USB1-as-full-speed-device/m-p/1680697#M53311</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I see in this topic...&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537&lt;/A&gt;&lt;/P&gt;&lt;P&gt;that USB1 can't be forced to device in full speed mode, but there is in user manual (UM11126),&amp;nbsp;Table 834. USB1 device command/status register (DEVCMDSTAT) bit 21 (R/W):&lt;/P&gt;&lt;P&gt;Forced FS&lt;/P&gt;&lt;P&gt;0: Default - drive K chirp during reset, go through HS negotiation.&lt;/P&gt;&lt;P&gt;1: Force the device to FS, do not drive K chirp during reset.&lt;/P&gt;&lt;P&gt;If USB1 device can be forced to full speed, in this case USB1 controller supporting crystal-less operation like USB0 or not? With both USB0 and USB1 active as full speed device.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JH&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 19:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-USB1-as-full-speed-device/m-p/1680697#M53311</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2023-07-03T19:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6x USB1 as full speed device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-USB1-as-full-speed-device/m-p/1682985#M53353</link>
      <description>&lt;P&gt;Hi&amp;nbsp;jh0&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you are right. USB1 can be used as Full speed. Forced FS value was updated in REV 2.4, 2021,OCT 07&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1688633122900.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/231083i7026613D27E7A01D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1688633122900.png" alt="ZhangJennie_0-1688633122900.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_0-1688633122900.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The thread you referred was posted in 2020. Please don't use it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jennie&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 08:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-USB1-as-full-speed-device/m-p/1682985#M53353</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-07-06T08:47:06Z</dc:date>
    </item>
  </channel>
</rss>