<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC546 MCAN Channel1 not working in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-MCAN-Channel1-not-working/m-p/1680671#M53310</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/122048"&gt;@emb02&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The CAN1 instance has different IRQ interrupt source value on the NVIC, please verify you are selecting the correct one. Look into &lt;STRONG&gt;Table&amp;nbsp;88. Connection of interrupt sources to the NVIC User Manual UM10912&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jul 2023 18:13:11 GMT</pubDate>
    <dc:creator>Miguel04</dc:creator>
    <dc:date>2023-07-03T18:13:11Z</dc:date>
    <item>
      <title>LPC546 MCAN Channel1 not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-MCAN-Channel1-not-working/m-p/1678673#M53283</link>
      <description>&lt;P&gt;Hello!&lt;BR /&gt;&lt;BR /&gt;I am using LPC546 development board with CANFD shield to implement MCAN protocol. I am initiating settings using configuration tools and using transfer mode.&lt;/P&gt;&lt;P&gt;I have use CAN0 channel which work perfectly fine but when I am using CAN1 channel with same settings IRQ is not enable,&amp;nbsp;I can't transmit or receive any CAN message as IRQ is not enabling. Is there any&amp;nbsp; specific settings&amp;nbsp;need to do in the peripheral?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 10:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-MCAN-Channel1-not-working/m-p/1678673#M53283</guid>
      <dc:creator>emb02</dc:creator>
      <dc:date>2023-06-29T10:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546 MCAN Channel1 not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-MCAN-Channel1-not-working/m-p/1680671#M53310</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/122048"&gt;@emb02&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The CAN1 instance has different IRQ interrupt source value on the NVIC, please verify you are selecting the correct one. Look into &lt;STRONG&gt;Table&amp;nbsp;88. Connection of interrupt sources to the NVIC User Manual UM10912&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 18:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-MCAN-Channel1-not-working/m-p/1680671#M53310</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-07-03T18:13:11Z</dc:date>
    </item>
  </channel>
</rss>