<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCU-LINK-PRO VCOM Voltage Range in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-LINK-PRO-VCOM-Voltage-Range/m-p/1676146#M53239</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I just wanted to get a clear answer on whether the VCOM port of the MCU-LINK-PRO Debug Probe can operate at both 3.3V and 1.8V. From the RM, I see that the SPI, I2C and triggering digital signals of the J19 header can be in the range of 1.2V-5.5V. However, I couldn't find any voltage specs for VCOM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it is able to receive and transmit UART data at 1.8V (assuming 3.3V is default), do I need to make any modifications (removing jumpers, etc...) for it to work?&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 15:59:58 GMT</pubDate>
    <dc:creator>LuisC</dc:creator>
    <dc:date>2023-06-26T15:59:58Z</dc:date>
    <item>
      <title>MCU-LINK-PRO VCOM Voltage Range</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-LINK-PRO-VCOM-Voltage-Range/m-p/1676146#M53239</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I just wanted to get a clear answer on whether the VCOM port of the MCU-LINK-PRO Debug Probe can operate at both 3.3V and 1.8V. From the RM, I see that the SPI, I2C and triggering digital signals of the J19 header can be in the range of 1.2V-5.5V. However, I couldn't find any voltage specs for VCOM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it is able to receive and transmit UART data at 1.8V (assuming 3.3V is default), do I need to make any modifications (removing jumpers, etc...) for it to work?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 15:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-LINK-PRO-VCOM-Voltage-Range/m-p/1676146#M53239</guid>
      <dc:creator>LuisC</dc:creator>
      <dc:date>2023-06-26T15:59:58Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-LINK-PRO VCOM Voltage Range</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-LINK-PRO-VCOM-Voltage-Range/m-p/1676238#M53240</link>
      <description>&lt;P&gt;See the schematics:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ErichStyger_0-1687798416108.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/229361i8819134391747140/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ErichStyger_0-1687798416108.png" alt="ErichStyger_0-1687798416108.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ErichStyger_0-1687798416108.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But be aware that the other UART pins are directly connected to the MCU (3.3V):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ErichStyger_1-1687798509050.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/229403i1FCF5143352A7F34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ErichStyger_1-1687798509050.png" alt="ErichStyger_1-1687798509050.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ErichStyger_1-1687798509050.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 16:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-LINK-PRO-VCOM-Voltage-Range/m-p/1676238#M53240</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-06-26T16:55:18Z</dc:date>
    </item>
  </channel>
</rss>