<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCommand Line mcuxpresso ide doesnt work when used in ci</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Command-Line-mcuxpresso-ide-doesnt-work-when-used-in-ci/m-p/1674178#M53173</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Following is the command line I use to run build my project&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;``&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; SET IDE_PATH=C:\nxp\MCUXpressoIDE_11.7.1_9221&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; SET IDE=%IDE_PATH%\ide\mcuxpressoidec.exe&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; mkdir workspace&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; "%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data workspace -import project&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; "%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data workspace -cleanBuild my_project/Release&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;``&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;This works fine, I have also placed sdk.zip in sdk_packages folder.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;The problem is when I use the same machine which I used to run these commands, as a CI agent/runnner(am using gitlab-ci/cd) at that time it throws me an error that it cannot find linker file and a ton of java errors. (These same errors were observed when I ran these commands on cmd_line locally and had forgot to place sdk.zip in its respective folder). But now that I have placed in the folder and it works locally, why does it fail when I use the same machine as CI agent/runner&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 22 Jun 2023 04:47:14 GMT</pubDate>
    <dc:creator>manasvb</dc:creator>
    <dc:date>2023-06-22T04:47:14Z</dc:date>
    <item>
      <title>Command Line mcuxpresso ide doesnt work when used in ci</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Command-Line-mcuxpresso-ide-doesnt-work-when-used-in-ci/m-p/1674178#M53173</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Following is the command line I use to run build my project&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;``&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; SET IDE_PATH=C:\nxp\MCUXpressoIDE_11.7.1_9221&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; SET IDE=%IDE_PATH%\ide\mcuxpressoidec.exe&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; mkdir workspace&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; "%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data workspace -import project&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; "%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data workspace -cleanBuild my_project/Release&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;``&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;This works fine, I have also placed sdk.zip in sdk_packages folder.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;The problem is when I use the same machine which I used to run these commands, as a CI agent/runnner(am using gitlab-ci/cd) at that time it throws me an error that it cannot find linker file and a ton of java errors. (These same errors were observed when I ran these commands on cmd_line locally and had forgot to place sdk.zip in its respective folder). But now that I have placed in the folder and it works locally, why does it fail when I use the same machine as CI agent/runner&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 22 Jun 2023 04:47:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Command-Line-mcuxpresso-ide-doesnt-work-when-used-in-ci/m-p/1674178#M53173</guid>
      <dc:creator>manasvb</dc:creator>
      <dc:date>2023-06-22T04:47:14Z</dc:date>
    </item>
    <item>
      <title>Re: Command Line mcuxpresso ide doesnt work when used in ci</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Command-Line-mcuxpresso-ide-doesnt-work-when-used-in-ci/m-p/1675847#M53232</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219083"&gt;@manasvb&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry I haven't test on CI, there is &amp;lt;MCUXpresso_IDE_Command_Line_User_Guide.pdf&amp;gt;, you can refer to, I attach it for you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 08:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Command-Line-mcuxpresso-ide-doesnt-work-when-used-in-ci/m-p/1675847#M53232</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-06-26T08:43:14Z</dc:date>
    </item>
  </channel>
</rss>