<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPCXpresso55S16 file system</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso55S16-file-system/m-p/1671900#M53075</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm looking for a sample usage of a file system on the on-chip internal flash of the LPCXpresso55S16. I attempted to use FatFs from the SDK, but I couldn't find an example despite downloading FatFs within the SDK. Additionally, I tried using littlefs, but encountered an error during the mounting process. It's possible that I'm using incorrect parameters or making other mistakes, as I only tried a basic example of mounting the file system without success.&lt;/P&gt;&lt;P&gt;I would greatly appreciate any assistance.&lt;/P&gt;&lt;P&gt;Thanks, Ahmed&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jun 2023 10:26:59 GMT</pubDate>
    <dc:creator>ahmed007</dc:creator>
    <dc:date>2023-06-19T10:26:59Z</dc:date>
    <item>
      <title>LPCXpresso55S16 file system</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso55S16-file-system/m-p/1671900#M53075</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm looking for a sample usage of a file system on the on-chip internal flash of the LPCXpresso55S16. I attempted to use FatFs from the SDK, but I couldn't find an example despite downloading FatFs within the SDK. Additionally, I tried using littlefs, but encountered an error during the mounting process. It's possible that I'm using incorrect parameters or making other mistakes, as I only tried a basic example of mounting the file system without success.&lt;/P&gt;&lt;P&gt;I would greatly appreciate any assistance.&lt;/P&gt;&lt;P&gt;Thanks, Ahmed&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 10:26:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso55S16-file-system/m-p/1671900#M53075</guid>
      <dc:creator>ahmed007</dc:creator>
      <dc:date>2023-06-19T10:26:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso55S16 file system</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso55S16-file-system/m-p/1672082#M53094</link>
      <description>&lt;P&gt;See your other question here: &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Littlefs-LPCXpresso55S16/m-p/1667540" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/Littlefs-LPCXpresso55S16/m-p/1667540&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 15:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso55S16-file-system/m-p/1672082#M53094</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-06-19T15:25:34Z</dc:date>
    </item>
  </channel>
</rss>